ZHCSB89H May 2013 – December 2021 TPS65310A-Q1
PRODUCTION DATA
PIN | TYPE(1) | PULLUP PULLDOWN |
DESCRIPTION | |
---|---|---|---|---|
NAME | NO. | |||
BOOT1 | 10 | I | — | The capacitor on these pins acts as the voltage supply for the high-side MOSFET gate-drive circuitry. |
BOOT2 | 29 | I | — | The capacitor on these pins act as the voltage supply for the high-side MOSFET gate drive circuitry. |
BOOT3 | 42 | I | — | The capacitor on these pins act as the voltage supply for the BUCK3 high-side MOSFET gate drive circuitry. |
COMP1 | 18 | O | — | Error amplifier output for the switching controller. External compensation network is connected to this node. |
COMP2 | 34 | I | — | Compensation selection for the BUCK2 switching converter |
COMP3 | 37 | I | — | Compensation selection for the BUCK3 switching converter. |
COMP5 | 20 | O | — | Error amplifier output for the boost switching controller. External compensation network is connected to this node. |
CSN | 44 | I | Pullup | SPI – Chip select |
DVDD | 55 | O | — | Internal DVDD output for decoupling |
EXTSUP | 8 | I | — | Optional LV input for gate driver supply |
GL | 13 | O | — | Gate driver – low-side FET |
GND | 56 | O | — | Analog GND, digital GND and substrate connection |
GPFET | 3 | O | — | Gate driver external protection PMOS FET. |
GU | 11 | O | — | Gate driver – high-side FET |
HSCTRL | 5 | O | — | High-side gate driver output |
HSPWM | 49 | I | Pulldown | High side and LED PWM input |
HSSENSE | 6 | I | — | Sense input high side and LED |
IRQ | 28 | OD | — | Low battery interrupt output in operating mode |
LDO | 51 | O | — | Linear regulated output (connect a low ESR ceramic output capacitor to this terminal) |
PGND1 | 14 | O | — | Ground for low-side FET driver |
PGND2 | 32 | O | — | Power ground of synchronous converter BUCK2 |
PGND3 | 39 | O | — | Power ground of synchronous converter BUCK3 |
PGND5 | 22 | O | — | Power ground boost converter |
PH1 | 12 | O | — | Switching node - BUCK1 (floating ground for high-side FET driver) |
PH2 | 31 | O | — | Switching node BUCK2 |
PH3 | 40 | O | — | Switching node BUCK3 |
PH5 | 23 | O | — | Switching node boost |
PRESN | 26 | OD | — | Peripherals reset |
RESN | 27 | OD | — | System reset |
S1 | 15 | I | — | Differential current sense inputs for BUCK1, S2 pull-down only active in RAMP and ACTIVE state |
S2 | 16 | I | Pulldown | |
SCK | 46 | I | Pulldown | SPI – Clock |
SDI | 45 | I | Pulldown | SPI – controller out, peripheral in |
SDO | 47 | O | — | SPI – controller in, peripheral out - push-pull output supplied by VIO |
VBOOST | 24 | I | — | Booster output voltage |
VIN | 2 | I | — | Unprotected supply input for the base functionality and band gap 1. Supplied blocks are: RESET, WD, wake, SPI, temp sensing, voltage monitoring and the logic block. |
VINPROT | 4 | I | — | Main input supply pin (gate drivers and bandgap2) |
VIO | 48 | I | — | Supply input for the digital interface to the MCU. Voltage on this input is monitored. If VIO falls below UV threshold a reset is generated and the part enters error mode. |
VMON1 | 17 | I | — | Input pin for the independent voltage monitor at BUCK1 |
VMON2 | 33 | I | — | Input pin for the independent voltage monitor at BUCK2 |
VMON3 | 38 | I | — | Input pin for the independent voltage monitor at BUCK3 |
VREF | 53 | O | — | Accurate reference voltage output for peripherals on the system (for example, ADC) |
VREG | 9 | O | — | Internal regulator for gate driver supply (decoupling) and VREF |
VSENSE1 | 19 | I | — | Input for externally sensed voltage of the output using a resistor divider network from their respective output line to ground. |
VSENSE2 | 35 | I | — | Input for externally sensed voltage of the output using a resistor divider network from their respective output line to ground |
VSENSE3 | 36 | I | — | Input for externally sensed voltage of the output using a resistor divider network from their respective output line to ground |
VSENSE4 | 52 | I | — | Input for externally sensed voltage of the output using a resistor divider network from their respective output line to ground. |
VSENSE5 | 21 | I | — | Input for externally sensed voltage of the boost output using a resistor divider network from their respective output line to ground. |
VSSENSE | 1 | I | — | Input to monitor the battery line for undervoltage conditions. UV is indicated by the IRQ pin. |
VSUP2 | 30 | I | — | Input voltage supply for switch mode regulator BUCK2 |
VSUP3 | 41 | I | — | Input voltage supply for switch mode regulator BUCK3 |
VSUP4 | 50 | I | — | Input voltage supply for linear regulator LDO |
VT | 54 | I | — | Input pin for the comparator with shutdown functionality. This input can be used to sense an external NTC resistor to shutdown the IC in case the ambient temperature is too high or too low. Tie to GND if not in use. |
VT_REF | 25 | O | — | Shutdown comparator reference output. Internally connected to DVDD, current-limited. When not in use can be connected to DVDD or left open. |
WAKE | 7 | I | Pulldown | Wake up input |
WD | 43 | I | Pulldown | Watchdog input pin. WD is the trigger input coming from the MCU. |