SPRS357D August 2006 – June 2020 TMS320F28044
PRODUCTION DATA.
Figure 6-17 shows the OSC and PLL block on the F28044.
Figure 6-17 OSC and PLL Block Diagram The on-chip oscillator circuit enables a crystal/resonator to be attached to the F28044 device using the X1 and X2 pins. If the on-chip oscillator is not used, an external oscillator can be used in either one of the following configurations:
The three possible input-clock configurations are shown in Figure 6-18 through Figure 6-20
Figure 6-18 Using a 3.3-V External Oscillator
Figure 6-19 Using a 1.8-V External Oscillator
Figure 6-20 Using the Internal Oscillator