ZHCS916I March 2009 – December 2018 TMP112
PRODUCTION DATA.
When the device is in shutdown mode, writing a 1 to the OS bit begins a single temperature conversion. During the conversion, the OS bit reads 0. The device returns to the SHUTDOWN state at the completion of the single conversion. For more information on the one-shot conversion mode, see the One-Shot/Conversion Ready Mode (OS) section.