ZHCS916I March 2009 – December 2018 TMP112
PRODUCTION DATA.
The first byte transmitted by the master is the slave address with the R/W bit low. The TMP112 family then acknowledges reception of a valid address. The next byte transmitted by the master is the pointer register. The TMP112 family then acknowledges reception of the pointer register byte. The next byte or bytes are written to the register addressed by the pointer register. The TMP112 family acknowledges reception of each data byte. The master can terminate data transfer by generating a START or STOP condition.