ZHCSR22A June 2021 – September 2022 LP876242-Q1
PRODUCTION DATA
In Level Mode, after MCU has set the start bit (bit ESM_MCU_START ), the ESM_MCU monitors its nERR_MCU input pin. The ESM _MCU detects an ESM-error when the voltage level on its input pin remains low for a time equal or longer than the deglitch-time tdegl_ESMx. When the ESM_MCU detects an ESM-error, it starts the ESM Error-Handling procedure as described in Section 7.3.9.1. The Error-Handling Procedure is stopped if, before elapse of the delay-1 or delay-2 interval, the voltage level on the input pin remains high for a time equal or longer than the deglitch-time tdegl_ESMx and the MCU clears all corresponding interrupt bits. If the ESM-error persists such that the configured delay-1 and delay-2 times elapse, the ESM_MCU sends a ESM_MCU_RST trigger to the PFSM and the device clear the ESM_MCU_START bit. After the PFSM completes the handling of the ESM_MCU_RST trigger, the device re-initializes the ESM_MCU.
For a complete overview on how the ESM_MCU works in Level Mode, please refer to the flow-chart in Figure 7-24. In this flow-chart, the _x stands for _MCU. Figure 7-25, Figure 7-26, Figure 7-27, and Figure 7-28 show example wave forms for several error-cases for the ESM_MCU in Level Mode.