ZHCS990C June 2012 – September 2021 TPS54719
PRODUCTION DATA
For the example design, 20.0 kΩ was selected for R6. Using Equation 31, R7 is calculated as 10.0 kΩ.
Due to the internal design of the TPS54719, there is a minimum output voltage limit for any given input voltage. The output voltage can never be lower than the internal voltage reference of 0.6 V. Above 0.6 V, the output voltage may be limited by the minimum controllable on time. The minimum output voltage in this case is given by Equation 32.
where:
There is also a maximum achievable output voltage which is limited by the minimum off time. The maximum output voltage is given by Equation 33
where: