ZHCSD20G October 2014 – November 2023 DLPC900
PRODUCTION DATA
Flash changes will require a change to the flash parameters file. This file must be changed to match the flash device info for the selected device including the sector mapping of the device.
Refer to the appropriate BOM for a list of flash memory that was used and tested on the DLP®LightCrafter™ Single DLPC900 Evaluation Module and DLP®LightCrafter™ Dual DLPC900 Evaluation Module. The reader can also refer to the datasheets for alternate package types for each of the components listed. If substituting other flash memory, the user must consult the datasheets to ensure compatibility.