SWRA446 February 2015 CC1310 , CC1310 , CC2620 , CC2620 , CC2630 , CC2630 , CC2640 , CC2640 , CC2640R2F , CC2640R2F , CC2640R2F-Q1 , CC2640R2F-Q1 , CC2650 , CC2650 , CC2650MODA , CC2650MODA
For Linux, the *.elf file that was generated in the previous section will be loaded to the target using the Uniflash Flash programming tool.
Load the binary image to the target by running the Flash Programmer tool: Run → External Tools → External Tools Configurations… . Select Flash program under 'Program' in the left side panel and click 'Run'. The console output should be similar to the output shown in Figure 19.
Figure 19. Load the Image to Target (Linux)