SWRA446 February 2015 CC1310 , CC1310 , CC2620 , CC2620 , CC2630 , CC2630 , CC2640 , CC2640 , CC2640R2F , CC2640R2F , CC2640R2F-Q1 , CC2640R2F-Q1 , CC2650 , CC2650 , CC2650MODA , CC2650MODA
The GDB Server agent is found in the folder where the TI EmuPack is installed. If it is installed in default directory, it can be found in the folder C:\ti\ccs_base\common\uscif. Perform the following steps to launch and configure the GDB Server for the XDS100v3 emulator on Windows:
Figure 20. Launching the GDB Server (Windows)