SWRA446 February 2015 CC1310 , CC1310 , CC2620 , CC2620 , CC2630 , CC2630 , CC2640 , CC2640 , CC2640R2F , CC2640R2F , CC2640R2F-Q1 , CC2640R2F-Q1 , CC2650 , CC2650 , CC2650MODA , CC2650MODA
The Eclipse IDE is dependent on the Java Runtime Environment (JRE) being installed on the machine. Note that both JRE and Eclipse must be downloaded for the same platform (the 64-bit version of Eclipse requires the 64-bit version of JRE). Make sure JRE is installed before performing installation of the Eclipse IDE. If not, it can be downloaded from http://java.com/en/download/index.jsp.