SWRA446 February 2015 CC1310 , CC1310 , CC2620 , CC2620 , CC2630 , CC2630 , CC2640 , CC2640 , CC2640R2F , CC2640R2F , CC2640R2F-Q1 , CC2640R2F-Q1 , CC2650 , CC2650 , CC2650MODA , CC2650MODA
The GDB server agent is found in the following folder where UniFlash is installed: ccs_base\common\uscif. Perform the following steps to launch and configure the GDB Server for the XDS100v3 emulator on Linux:
gdb_agent_console <board-data-file>
The board-data-file is the *.dat file found in the software example package: CC26xx_XDS100v3c2_linux.dat.
Figure 21. Launching the GDB Server (Linux)