SWCU185G January 2018 – June 2024 CC1312PSIP , CC1312R , CC1352P , CC1352R , CC2642R , CC2642R-Q1 , CC2652P , CC2652PSIP , CC2652R , CC2652RB , CC2652RSIP , CC2662R-Q1
A master radio operation is started by a CMD_BLE_MASTER or a CMD_BLE5_MASTER command. In the command structure, it shall have a pParams parameter of the type defined in Table 26-97 and a pOutput parameter of the type defined in Table 26-109. The operation starts with transmission. After each transmission, the receiver is started.
A master operation shall end by one of the causes listed in Table 26-131. The status field of the command structure after the operation is ended indicates the reason why the operation ended. In all cases, a Command_Done interrupt is raised. In each case, the result of TRUE, FALSE, or ABORT is indicated, which will decide the next action.
| Condition | Status Code | Result |
|---|---|---|
| Successfully received packet with MD = 0 after transmitting a packet with MD = 0 | BLE_DONE_OK | TRUE |
| Received packet that did not fit in RX queue after transmitting a packet with MD = 0 | BLE_DONE_OK | TRUE |
| Received a packet after nPkt had counted to 0 | BLE_DONE_OK | TRUE |
| No sync obtained on receive operation after transmit | BLE_DONE_NOSYNC | TRUE |
| Two subsequent packets in the same operation were received with CRC error | BLE_DONE_RXERR | TRUE |
| The internal counter nNack counted down to 0 after a packet was received | BLE_DONE_MAXNACK | TRUE |
| Received a packet after observing a trigger indicated by pParams->endTrigger | BLE_DONE_ENDED | FALSE |
| Received a packet after observing a CMD_STOP | BLE_DONE_STOPPED | FALSE |
| Received CMD_ABORT | BLE_DONE_ABORT | ABORT |
| Illegal value of channel | BLE_ERROR_PAR | ABORT |
| TX data entry length field has illegal value | BLE_ERROR_PAR | ABORT |