SWCU185G January 2018 ā June 2024 CC1312PSIP , CC1312R , CC1352P , CC1352R , CC2642R , CC2642R-Q1 , CC2652P , CC2652PSIP , CC2652R , CC2652RB , CC2652RSIP , CC2662R-Q1
Table 20-113 lists the memory-mapped registers for the AUX_TDC registers. All register offset addresses not listed in Table 20-113 should be considered as reserved locations and the register contents should not be modified.
| Offset | Acronym | Register Name | Section |
|---|---|---|---|
| 0h | CTL | Control | CTL Register (Offset = 0h) [Reset = 00000000h] |
| 4h | STAT | Status | STAT Register (Offset = 4h) [Reset = 00000006h] |
| 8h | RESULT | Result | RESULT Register (Offset = 8h) [Reset = 00000002h] |
| Ch | SATCFG | Saturation Configuration | SATCFG Register (Offset = Ch) [Reset = 0000000Fh] |
| 10h | TRIGSRC | Trigger Source | TRIGSRC Register (Offset = 10h) [Reset = 00000000h] |
| 14h | TRIGCNT | Trigger Counter | TRIGCNT Register (Offset = 14h) [Reset = 00000000h] |
| 18h | TRIGCNTLOAD | Trigger Counter Load | TRIGCNTLOAD Register (Offset = 18h) [Reset = 00000000h] |
| 1Ch | TRIGCNTCFG | Trigger Counter Configuration | TRIGCNTCFG Register (Offset = 1Ch) [Reset = 00000000h] |
| 20h | PRECTL | Prescaler Control | PRECTL Register (Offset = 20h) [Reset = 0000003Fh] |
| 24h | PRECNTR | Prescaler Counter | PRECNTR Register (Offset = 24h) [Reset = 00000000h] |
Complex bit access types are encoded to fit into small table cells. Table 20-114 shows the codes that are used for access types in this section.
| Access Type | Code | Description |
|---|---|---|
| Read Type | ||
| R | R | Read |
| Write Type | ||
| W | W | Write |
| Reset or Default Value | ||
| -n | Value after reset or the default value | |
CTL is shown in Figure 20-101 and described in Table 20-115.
Return to the Summary Table.
Control
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||||||||||
| R-0h | |||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | CMD | ||||||||||||||
| R-0h | W-0h | ||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-2 | RESERVED | R | 0h | Reserved |
| 1-0 | CMD | W | 0h | TDC commands.
0h = Clear STAT.SAT, STAT.DONE, and RESULT.VALUE. This is not needed as prerequisite for a measurement. Reliable clear is only guaranteed from IDLE state. 1h = Synchronous counter start. The counter looks for the opposite edge of the selected start event before it starts to count when the selected edge occurs. This guarantees an edge-triggered start and is recommended for frequency measurements. 2h = Asynchronous counter start. The counter starts to count when the start event is high. To achieve precise edge-to-edge measurements you must ensure that the start event is low for at least 420 ns after you write this command. 3h = Force TDC state machine back to IDLE state. Never write this command while AUX_TDC:STAT.STATE equals CLR_CNT or WAIT_CLR_CNT_DONE. |
STAT is shown in Figure 20-102 and described in Table 20-116.
Return to the Summary Table.
Status
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| SAT | DONE | STATE | |||||
| R-0h | R-0h | R-6h | |||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-8 | RESERVED | R | 0h | Reserved |
| 7 | SAT | R | 0h | TDC measurement saturation flag. 0: Conversion has not saturated. 1: Conversion stopped due to saturation. This field is cleared when a new measurement is started or when CLR_RESULT is written to CTL.CMD. |
| 6 | DONE | R | 0h | TDC measurement complete flag. 0: TDC measurement has not yet completed. 1: TDC measurement has completed. This field clears when a new TDC measurement starts or when you write CLR_RESULT to CTL.CMD. |
| 5-0 | STATE | R | 6h | TDC state machine status.
0h = Current state is TDC_STATE_WAIT_START. The fast-counter circuit looks for the start condition. The state machine waits for the fast-counter to increment. 4h = Current state is TDC_STATE_WAIT_STARTSTOPCNTEN. The fast-counter circuit looks for the start condition. The state machine waits for the fast-counter to increment. 6h = Current state is TDC_STATE_IDLE. This is the default state after reset and abortion. State will change when you write CTL.CMD to either RUN_SYNC_START or RUN. 7h = Current state is TDC_STATE_CLRCNT. The fast-counter circuit is reset. 8h = Current state is TDC_STATE_WAIT_STOP. The state machine waits for the fast-counter circuit to stop. Ch = Current state is TDC_STATE_WAIT_STOPCNTDOWN. The fast-counter circuit looks for the stop condition. It will ignore a number of stop events configured in TRIGCNTLOAD.CNT. Eh = Current state is TDC_STATE_GETRESULTS. The state machine copies the counter value from the fast-counter circuit. Fh = Current state is TDC_STATE_POR. This is the reset state. 16h = Current state is TDC_STATE_WAIT_CLRCNT_DONE. The state machine waits for fast-counter circuit to finish reset. 1Eh = Current state is TDC_WAIT_STARTFALL. The fast-counter circuit waits for a falling edge on the start event. 2Eh = Current state is TDC_FORCESTOP. You wrote ABORT to CTL.CMD to abort the TDC measurement. |
RESULT is shown in Figure 20-103 and described in Table 20-117.
Return to the Summary Table.
Result
Result of last TDC conversion.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | VALUE | ||||||||||||||
| R-0h | R-2h | ||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| VALUE | |||||||||||||||
| R-2h | |||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-25 | RESERVED | R | 0h | Reserved |
| 24-0 | VALUE | R | 2h | TDC conversion result. The result of the TDC conversion is given in number of clock edges of the clock source selected in DDI_0_OSC:CTL0.ACLK_TDC_SRC_SEL. Both rising and falling edges are counted. If TDC counter saturates, VALUE is slightly higher than SATCFG.LIMIT, as it takes a non-zero time to stop the measurement. Hence, the maximum value of this field becomes slightly higher than 224 if you configure SATCFG.LIMIT to R24. |
SATCFG is shown in Figure 20-104 and described in Table 20-118.
Return to the Summary Table.
Saturation Configuration
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||||||||||
| R-0h | |||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | LIMIT | ||||||||||||||
| R-0h | R/W-Fh | ||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-4 | RESERVED | R | 0h | Reserved |
| 3-0 | LIMIT | R/W | Fh | Saturation limit. The flag STAT.SAT is set when the TDC counter saturates. Values not enumerated are not supported 3h = Result bit 12: TDC conversion saturates and stops when RESULT.VALUE[12] is set. 4h = Result bit 13: TDC conversion saturates and stops when RESULT.VALUE[13] is set. 5h = Result bit 14: TDC conversion saturates and stops when RESULT.VALUE[14] is set. 6h = Result bit 15: TDC conversion saturates and stops when RESULT.VALUE[15] is set. 7h = Result bit 16: TDC conversion saturates and stops when RESULT.VALUE[16] is set. 8h = Result bit 17: TDC conversion saturates and stops when RESULT.VALUE[17] is set. 9h = Result bit 18: TDC conversion saturates and stops when RESULT.VALUE[18] is set. Ah = Result bit 19: TDC conversion saturates and stops when RESULT.VALUE[19] is set. Bh = Result bit 20: TDC conversion saturates and stops when RESULT.VALUE[20] is set. Ch = Result bit 21: TDC conversion saturates and stops when RESULT.VALUE[21] is set. Dh = Result bit 22: TDC conversion saturates and stops when RESULT.VALUE[22] is set. Eh = Result bit 23: TDC conversion saturates and stops when RESULT.VALUE[23] is set. Fh = Result bit 24: TDC conversion saturates and stops when RESULT.VALUE[24] is set. |
TRIGSRC is shown in Figure 20-105 and described in Table 20-119.
Return to the Summary Table.
Trigger Source
Select source and polarity for TDC start and stop events. See the Technical Reference Manual for event timing requirements.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | STOP_POL | STOP_SRC | |||||
| R-0h | R/W-0h | R/W-0h | |||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | START_POL | START_SRC | |||||
| R-0h | R/W-0h | R/W-0h | |||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-15 | RESERVED | R | 0h | Reserved |
| 14 | STOP_POL | R/W | 0h | Polarity of stop source. Change only while STAT.STATE is IDLE. 0h = TDC conversion stops when high level is detected. 1h = TDC conversion stops when low level is detected. |
| 13-8 | STOP_SRC | R/W | 0h | Select stop source from the asynchronous AUX event bus. Change only while STAT.STATE is IDLE. 0h = AUX_EVCTL:EVSTAT0.AUXIO0 1h = AUX_EVCTL:EVSTAT0.AUXIO1 2h = AUX_EVCTL:EVSTAT0.AUXIO2 3h = AUX_EVCTL:EVSTAT0.AUXIO3 4h = AUX_EVCTL:EVSTAT0.AUXIO4 5h = AUX_EVCTL:EVSTAT0.AUXIO5 6h = AUX_EVCTL:EVSTAT0.AUXIO6 7h = AUX_EVCTL:EVSTAT0.AUXIO7 8h = AUX_EVCTL:EVSTAT0.AUXIO8 9h = AUX_EVCTL:EVSTAT0.AUXIO9 Ah = AUX_EVCTL:EVSTAT0.AUXIO10 Bh = AUX_EVCTL:EVSTAT0.AUXIO11 Ch = AUX_EVCTL:EVSTAT0.AUXIO12 Dh = AUX_EVCTL:EVSTAT0.AUXIO13 Eh = AUX_EVCTL:EVSTAT0.AUXIO14 Fh = AUX_EVCTL:EVSTAT0.AUXIO15 10h = AUX_EVCTL:EVSTAT1.AUXIO16 11h = AUX_EVCTL:EVSTAT1.AUXIO17 12h = AUX_EVCTL:EVSTAT1.AUXIO18 13h = AUX_EVCTL:EVSTAT1.AUXIO19 14h = AUX_EVCTL:EVSTAT1.AUXIO20 15h = AUX_EVCTL:EVSTAT1.AUXIO21 16h = AUX_EVCTL:EVSTAT1.AUXIO22 17h = AUX_EVCTL:EVSTAT1.AUXIO23 18h = AUX_EVCTL:EVSTAT1.AUXIO24 19h = AUX_EVCTL:EVSTAT1.AUXIO25 1Ah = AUX_EVCTL:EVSTAT1.AUXIO26 1Bh = AUX_EVCTL:EVSTAT1.AUXIO27 1Ch = AUX_EVCTL:EVSTAT1.AUXIO28 1Dh = AUX_EVCTL:EVSTAT1.AUXIO29 1Eh = AUX_EVCTL:EVSTAT1.AUXIO30 1Fh = AUX_EVCTL:EVSTAT1.AUXIO31 20h = AUX_EVCTL:EVSTAT2.MANUAL_EV 21h = AUX_EVCTL:EVSTAT2.AON_RTC_CH2 22h = AUX_EVCTL:EVSTAT2.AON_RTC_CH2_DLY 23h = AUX_EVCTL:EVSTAT2.AON_RTC_4KHZ 24h = AUX_EVCTL:EVSTAT2.AON_BATMON_BAT_UPD 25h = AUX_EVCTL:EVSTAT2.AON_BATMON_TEMP_UPD 26h = AUX_EVCTL:EVSTAT2.SCLK_LF 27h = AUX_EVCTL:EVSTAT2.PWR_DWN 28h = AUX_EVCTL:EVSTAT2.MCU_ACTIVE 29h = AUX_EVCTL:EVSTAT2.VDDR_RECHARGE 2Ah = AUX_EVCTL:EVSTAT2.ACLK_REF 2Bh = AUX_EVCTL:EVSTAT2.MCU_EV 2Ch = AUX_EVCTL:EVSTAT2.MCU_OBSMUX0 2Dh = AUX_EVCTL:EVSTAT2.MCU_OBSMUX1 2Eh = AUX_EVCTL:EVSTAT2.AUX_COMPA 2Fh = AUX_EVCTL:EVSTAT2.AUX_COMPB 30h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV0 31h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV1 32h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV2 33h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV3 34h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_PULSE 35h = AUX_EVCTL:EVSTAT3.AUX_TIMER1_EV 36h = AUX_EVCTL:EVSTAT3.AUX_TIMER0_EV 37h = AUX_EVCTL:EVSTAT3.AUX_TDC_DONE 38h = AUX_EVCTL:EVSTAT3.AUX_ISRC_RESET_N 39h = AUX_EVCTL:EVSTAT3.AUX_ADC_DONE 3Ah = AUX_EVCTL:EVSTAT3.AUX_ADC_IRQ 3Bh = AUX_EVCTL:EVSTAT3.AUX_ADC_FIFO_ALMOST_FULL 3Ch = AUX_EVCTL:EVSTAT3.AUX_ADC_FIFO_NOT_EMPTY 3Dh = AUX_EVCTL:EVSTAT3.AUX_SMPH_AUTOTAKE_DONE 3Eh = Select TDC Prescaler event which is generated by configuration of PRECTL. 3Fh = No event. |
| 7 | RESERVED | R | 0h | Reserved |
| 6 | START_POL | R/W | 0h | Polarity of start source. Change only while STAT.STATE is IDLE. 0h = TDC conversion starts when high level is detected. 1h = TDC conversion starts when low level is detected. |
| 5-0 | START_SRC | R/W | 0h | Select start source from the asynchronous AUX event bus. Change only while STAT.STATE is IDLE. 0h = AUX_EVCTL:EVSTAT0.AUXIO0 1h = AUX_EVCTL:EVSTAT0.AUXIO1 2h = AUX_EVCTL:EVSTAT0.AUXIO2 3h = AUX_EVCTL:EVSTAT0.AUXIO3 4h = AUX_EVCTL:EVSTAT0.AUXIO4 5h = AUX_EVCTL:EVSTAT0.AUXIO5 6h = AUX_EVCTL:EVSTAT0.AUXIO6 7h = AUX_EVCTL:EVSTAT0.AUXIO7 8h = AUX_EVCTL:EVSTAT0.AUXIO8 9h = AUX_EVCTL:EVSTAT0.AUXIO9 Ah = AUX_EVCTL:EVSTAT0.AUXIO10 Bh = AUX_EVCTL:EVSTAT0.AUXIO11 Ch = AUX_EVCTL:EVSTAT0.AUXIO12 Dh = AUX_EVCTL:EVSTAT0.AUXIO13 Eh = AUX_EVCTL:EVSTAT0.AUXIO14 Fh = AUX_EVCTL:EVSTAT0.AUXIO15 10h = AUX_EVCTL:EVSTAT1.AUXIO16 11h = AUX_EVCTL:EVSTAT1.AUXIO17 12h = AUX_EVCTL:EVSTAT1.AUXIO18 13h = AUX_EVCTL:EVSTAT1.AUXIO19 14h = AUX_EVCTL:EVSTAT1.AUXIO20 15h = AUX_EVCTL:EVSTAT1.AUXIO21 16h = AUX_EVCTL:EVSTAT1.AUXIO22 17h = AUX_EVCTL:EVSTAT1.AUXIO23 18h = AUX_EVCTL:EVSTAT1.AUXIO24 19h = AUX_EVCTL:EVSTAT1.AUXIO25 1Ah = AUX_EVCTL:EVSTAT1.AUXIO26 1Bh = AUX_EVCTL:EVSTAT1.AUXIO27 1Ch = AUX_EVCTL:EVSTAT1.AUXIO28 1Dh = AUX_EVCTL:EVSTAT1.AUXIO29 1Eh = AUX_EVCTL:EVSTAT1.AUXIO30 1Fh = AUX_EVCTL:EVSTAT1.AUXIO31 20h = AUX_EVCTL:EVSTAT2.MANUAL_EV 21h = AUX_EVCTL:EVSTAT2.AON_RTC_CH2 22h = AUX_EVCTL:EVSTAT2.AON_RTC_CH2_DLY 23h = AUX_EVCTL:EVSTAT2.AON_RTC_4KHZ 24h = AUX_EVCTL:EVSTAT2.AON_BATMON_BAT_UPD 25h = AUX_EVCTL:EVSTAT2.AON_BATMON_TEMP_UPD 26h = AUX_EVCTL:EVSTAT2.SCLK_LF 27h = AUX_EVCTL:EVSTAT2.PWR_DWN 28h = AUX_EVCTL:EVSTAT2.MCU_ACTIVE 29h = AUX_EVCTL:EVSTAT2.VDDR_RECHARGE 2Ah = AUX_EVCTL:EVSTAT2.ACLK_REF 2Bh = AUX_EVCTL:EVSTAT2.MCU_EV 2Ch = AUX_EVCTL:EVSTAT2.MCU_OBSMUX0 2Dh = AUX_EVCTL:EVSTAT2.MCU_OBSMUX1 2Eh = AUX_EVCTL:EVSTAT2.AUX_COMPA 2Fh = AUX_EVCTL:EVSTAT2.AUX_COMPB 30h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV0 31h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV1 32h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV2 33h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV3 34h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_PULSE 35h = AUX_EVCTL:EVSTAT3.AUX_TIMER1_EV 36h = AUX_EVCTL:EVSTAT3.AUX_TIMER0_EV 37h = AUX_EVCTL:EVSTAT3.AUX_TDC_DONE 38h = AUX_EVCTL:EVSTAT3.AUX_ISRC_RESET_N 39h = AUX_EVCTL:EVSTAT3.AUX_ADC_DONE 3Ah = AUX_EVCTL:EVSTAT3.AUX_ADC_IRQ 3Bh = AUX_EVCTL:EVSTAT3.AUX_ADC_FIFO_ALMOST_FULL 3Ch = AUX_EVCTL:EVSTAT3.AUX_ADC_FIFO_NOT_EMPTY 3Dh = AUX_EVCTL:EVSTAT3.AUX_SMPH_AUTOTAKE_DONE 3Eh = Select TDC Prescaler event which is generated by configuration of PRECTL. 3Fh = No event. |
TRIGCNT is shown in Figure 20-106 and described in Table 20-120.
Return to the Summary Table.
Trigger Counter
Stop-counter control and status.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | CNT | ||||||||||||||||||||||||||||||
| R-0h | R/W-0h | ||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | CNT | R/W | 0h | Number of stop events to ignore when AUX_TDC:TRIGCNTCFG.EN is 1. Read CNT to get the remaining number of stop events to ignore during a TDC measurement. Write CNT to update the remaining number of stop events to ignore during a TDC measurement. The TDC measurement ignores updates of CNT if there are no more stop events left to ignore. When AUX_TDC:TRIGCNTCFG.EN is 1, TRIGCNTLOAD.CNT is loaded into CNT at the start of the measurement. |
TRIGCNTLOAD is shown in Figure 20-107 and described in Table 20-121.
Return to the Summary Table.
Trigger Counter Load
Stop-counter load.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | CNT | ||||||||||||||||||||||||||||||
| R-0h | R/W-0h | ||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | CNT | R/W | 0h | Number of stop events to ignore when AUX_TDC:TRIGCNTCFG.EN is 1. To measure frequency of an event source: - Set start event equal to stop event. - Set CNT to number of periods to measure. Both 0 and 1 values measures a single event source period. To measure pulse width of an event source: - Set start event source equal to stop event source. - Select different polarity for start and stop event. - Set CNT to 0. To measure time from the start event to the Nth stop event when N > 1: - Select different start and stop event source. - Set CNT to (N-1). See the Technical Reference Manual for event timing requirements. When AUX_TDC:TRIGCNTCFG.EN is 1, CNT is loaded into TRIGCNT.CNT at the start of the measurement. |
TRIGCNTCFG is shown in Figure 20-108 and described in Table 20-122.
Return to the Summary Table.
Trigger Counter Configuration
Stop-counter configuration.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||||||||||
| R-0h | |||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | EN | ||||||||||||||
| R-0h | R/W-0h | ||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-1 | RESERVED | R | 0h | Reserved |
| 0 | EN | R/W | 0h | Enable stop-counter. 0: Disable stop-counter. 1: Enable stop-counter. Change only while STAT.STATE is IDLE. |
PRECTL is shown in Figure 20-109 and described in Table 20-123.
Return to the Summary Table.
Prescaler Control
The prescaler can be used to count events that are faster than the AUX bus rate.
It can be used to:
- count pulses on a specified event from the asynchronous event bus.
- prescale a specified event from the asynchronous event bus.
To use the prescaler output as an event source in TDC measurements you must set both TRIGSRC.START_SRC and TRIGSRC.STOP_SRC to AUX_TDC_PRE.
It is recommended to use the prescaler when the signal frequency to measure exceeds 1/10th of the AUX bus rate.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESET_N | RATIO | SRC | |||||
| R/W-0h | R/W-0h | R/W-3Fh | |||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-8 | RESERVED | R | 0h | Reserved |
| 7 | RESET_N | R/W | 0h | Prescaler reset. 0: Reset prescaler. 1: Release reset of prescaler. AUX_TDC_PRE event becomes 0 when you reset the prescaler. |
| 6 | RATIO | R/W | 0h | Prescaler ratio. This controls how often the AUX_TDC_PRE event is generated by the prescaler. 0h = Prescaler divides input by 16. AUX_TDC_PRE event has a rising edge for every 16 rising edges of the input. AUX_TDC_PRE event toggles on every 8th rising edge of the input. 1h = Prescaler divides input by 64. AUX_TDC_PRE event has a rising edge for every 64 rising edges of the input. AUX_TDC_PRE event toggles on every 32nd rising edge of the input. |
| 5-0 | SRC | R/W | 3Fh | Prescaler event source. Select an event from the asynchronous AUX event bus to connect to the prescaler input. Configure only while RESET_N is 0. 0h = AUX_EVCTL:EVSTAT0.AUXIO0 1h = AUX_EVCTL:EVSTAT0.AUXIO1 2h = AUX_EVCTL:EVSTAT0.AUXIO2 3h = AUX_EVCTL:EVSTAT0.AUXIO3 4h = AUX_EVCTL:EVSTAT0.AUXIO4 5h = AUX_EVCTL:EVSTAT0.AUXIO5 6h = AUX_EVCTL:EVSTAT0.AUXIO6 7h = AUX_EVCTL:EVSTAT0.AUXIO7 8h = AUX_EVCTL:EVSTAT0.AUXIO8 9h = AUX_EVCTL:EVSTAT0.AUXIO9 Ah = AUX_EVCTL:EVSTAT0.AUXIO10 Bh = AUX_EVCTL:EVSTAT0.AUXIO11 Ch = AUX_EVCTL:EVSTAT0.AUXIO12 Dh = AUX_EVCTL:EVSTAT0.AUXIO13 Eh = AUX_EVCTL:EVSTAT0.AUXIO14 Fh = AUX_EVCTL:EVSTAT0.AUXIO15 10h = AUX_EVCTL:EVSTAT1.AUXIO16 11h = AUX_EVCTL:EVSTAT1.AUXIO17 12h = AUX_EVCTL:EVSTAT1.AUXIO18 13h = AUX_EVCTL:EVSTAT1.AUXIO19 14h = AUX_EVCTL:EVSTAT1.AUXIO20 15h = AUX_EVCTL:EVSTAT1.AUXIO21 16h = AUX_EVCTL:EVSTAT1.AUXIO22 17h = AUX_EVCTL:EVSTAT1.AUXIO23 18h = AUX_EVCTL:EVSTAT1.AUXIO24 19h = AUX_EVCTL:EVSTAT1.AUXIO25 1Ah = AUX_EVCTL:EVSTAT1.AUXIO26 1Bh = AUX_EVCTL:EVSTAT1.AUXIO27 1Ch = AUX_EVCTL:EVSTAT1.AUXIO28 1Dh = AUX_EVCTL:EVSTAT1.AUXIO29 1Eh = AUX_EVCTL:EVSTAT1.AUXIO30 1Fh = AUX_EVCTL:EVSTAT1.AUXIO31 20h = AUX_EVCTL:EVSTAT2.MANUAL_EV 21h = AUX_EVCTL:EVSTAT2.AON_RTC_CH2 22h = AUX_EVCTL:EVSTAT2.AON_RTC_CH2_DLY 23h = AUX_EVCTL:EVSTAT2.AON_RTC_4KHZ 24h = AUX_EVCTL:EVSTAT2.AON_BATMON_BAT_UPD 25h = AUX_EVCTL:EVSTAT2.AON_BATMON_TEMP_UPD 26h = AUX_EVCTL:EVSTAT2.SCLK_LF 27h = AUX_EVCTL:EVSTAT2.PWR_DWN 28h = AUX_EVCTL:EVSTAT2.MCU_ACTIVE 29h = AUX_EVCTL:EVSTAT2.VDDR_RECHARGE 2Ah = AUX_EVCTL:EVSTAT2.ACLK_REF 2Bh = AUX_EVCTL:EVSTAT2.MCU_EV 2Ch = AUX_EVCTL:EVSTAT2.MCU_OBSMUX0 2Dh = AUX_EVCTL:EVSTAT2.MCU_OBSMUX1 2Eh = AUX_EVCTL:EVSTAT2.AUX_COMPA 2Fh = AUX_EVCTL:EVSTAT2.AUX_COMPB 30h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV0 31h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV1 32h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV2 33h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV3 34h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_PULSE 35h = AUX_EVCTL:EVSTAT3.AUX_TIMER1_EV 36h = AUX_EVCTL:EVSTAT3.AUX_TIMER0_EV 37h = AUX_EVCTL:EVSTAT3.AUX_TDC_DONE 38h = AUX_EVCTL:EVSTAT3.AUX_ISRC_RESET_N 39h = AUX_EVCTL:EVSTAT3.AUX_ADC_DONE 3Ah = AUX_EVCTL:EVSTAT3.AUX_ADC_IRQ 3Bh = AUX_EVCTL:EVSTAT3.AUX_ADC_FIFO_ALMOST_FULL 3Ch = AUX_EVCTL:EVSTAT3.AUX_ADC_FIFO_NOT_EMPTY 3Dh = AUX_EVCTL:EVSTAT3.AUX_SMPH_AUTOTAKE_DONE 3Fh = No event. |
PRECNTR is shown in Figure 20-110 and described in Table 20-124.
Return to the Summary Table.
Prescaler Counter
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | CNT | ||||||||||||||||||||||||||||||
| R-0h | R/W-0h | ||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | CNT | R/W | 0h | Prescaler counter value. Write a value to CNT to capture the value of the 16-bit prescaler counter into CNT. Read CNT to get the captured value. The read value gets 1 LSB uncertainty if the event source level rises when you release the reset. The read value gets 1 LSB uncertainty if the event source level rises when you capture the prescaler counter. Please note the following: - The prescaler counter is reset to 2 by PRECTL.RESET_N. - The captured value is 2 when the number of rising edges on prescaler input is less than 3. Otherwise, captured value equals number of event pulses - 1. |