SWCU185G January 2018 – June 2024 CC1312PSIP , CC1312R , CC1352P , CC1352R , CC2642R , CC2642R-Q1 , CC2652P , CC2652PSIP , CC2652R , CC2652RB , CC2652RSIP , CC2662R-Q1
Table 8-8 lists the memory-mapped registers for the DDI_0_OSC registers. All register offset addresses not listed in Table 8-8 should be considered as reserved locations and the register contents should not be modified.
Complex bit access types are encoded to fit into small table cells. Table 8-9 shows the codes that are used for access types in this section.
| Access Type | Code | Description |
|---|---|---|
| Read Type | ||
| R | R | Read |
| Write Type | ||
| W | W | Write |
| Reset or Default Value | ||
| -n | Value after reset or the default value | |
CTL0 is shown in Figure 8-7 and described in Table 8-10.
Return to the Summary Table.
Control 0
Controls clock source selects
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| XTAL_IS_24M | RESERVED | BYPASS_XOSC_LF_CLK_QUAL | BYPASS_RCOSC_LF_CLK_QUAL | DOUBLER_START_DURATION | DOUBLER_RESET_DURATION | CLK_DCDC_SRC_SEL | |
| R/W-0h | R-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | |
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | HPOSC_MODE_EN | RESERVED | RCOSC_LF_TRIMMED | XOSC_HF_POWER_MODE | XOSC_LF_DIG_BYPASS | CLK_LOSS_EN | ACLK_TDC_SRC_SEL |
| R-0h | R/W-0h | R-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| ACLK_TDC_SRC_SEL | ACLK_REF_SRC_SEL | SCLK_LF_SRC_SEL | RESERVED | SCLK_HF_SRC_SEL | |||
| R/W-0h | R/W-0h | R/W-0h | R-0h | R/W-0h | |||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31 | XTAL_IS_24M | R/W | 0h | Set based on the accurate high frequency XTAL. |
| 30 | RESERVED | R | 0h | Reserved |
| 29 | BYPASS_XOSC_LF_CLK_QUAL | R/W | 0h | Internal. Only to be used through TI provided API. |
| 28 | BYPASS_RCOSC_LF_CLK_QUAL | R/W | 0h | Internal. Only to be used through TI provided API. |
| 27-26 | DOUBLER_START_DURATION | R/W | 0h | Internal. Only to be used through TI provided API. |
| 25 | DOUBLER_RESET_DURATION | R/W | 0h | Internal. Only to be used through TI provided API. |
| 24 | CLK_DCDC_SRC_SEL | R/W | 0h | Select DCDC clock source. 0: CLK_DCDC is 48 MHz clock from RCOSC or XOSC / HPOSC 1: CLK_DCDC is always 48 MHz clock from RCOSC |
| 23-15 | RESERVED | R | 0h | Reserved |
| 14 | HPOSC_MODE_EN | R/W | 0h | 0: HPOSC mode is not enabled. The 48 MHz crystal is required for radio operation. 1: Enables HPOSC mode. The internal HPOSC can be used as HF system clock and for radio operation. |
| 13 | RESERVED | R | 0h | Reserved |
| 12 | RCOSC_LF_TRIMMED | R/W | 0h | Internal. Only to be used through TI provided API. |
| 11 | XOSC_HF_POWER_MODE | R/W | 0h | Internal. Only to be used through TI provided API. |
| 10 | XOSC_LF_DIG_BYPASS | R/W | 0h | Bypass XOSC_LF and use the digital input clock from AON for the xosc_lf clock. 0: Use 32kHz XOSC as xosc_lf clock source 1: Use digital input (from AON) as xosc_lf clock source. This bit will only have effect when SCLK_LF_SRC_SEL is selecting the xosc_lf as the sclk_lf source. The muxing performed by this bit is not glitch free. The following procedure must be followed when changing this field to avoid glitches on sclk_lf. 1) Set SCLK_LF_SRC_SEL to select any source other than the xosc_lf clock source. 2) Set or clear this bit to bypass or not bypass the xosc_lf. 3) Set SCLK_LF_SRC_SEL to use xosc_lf. It is recommended that either the rcosc_hf or xosc_hf (whichever is currently active) be selected as the source in step 1 above. This provides a faster clock change. |
| 9 | CLK_LOSS_EN | R/W | 0h | Enable clock loss detection and hence the indicators to the system controller. Checks both SCLK_HF, SCLK_MF and SCLK_LF clock loss indicators. 0: Disable 1: Enable Clock loss detection must be disabled when changing the sclk_lf source. STAT0.SCLK_LF_SRC can be polled to determine when a change to a new sclk_lf source has completed. |
| 8-7 | ACLK_TDC_SRC_SEL | R/W | 0h | Source select for aclk_tdc. 00: RCOSC_HF (48MHz) 01: RCOSC_HF (24MHz) 10: XOSC_HF (24MHz) 11: Not used |
| 6-4 | ACLK_REF_SRC_SEL | R/W | 0h | Source select for aclk_ref 000: RCOSC_HF derived (31.25kHz) 001: XOSC_HF derived (31.25kHz) 010: RCOSC_LF (32kHz) 011: XOSC_LF (32.768kHz) 100: RCOSC_MF (2MHz) 101-111: Not used |
| 3-2 | SCLK_LF_SRC_SEL | R/W | 0h | Source select for sclk_lf
0h = Low frequency clock derived from High Frequency RCOSC 1h = Low frequency clock derived from High Frequency XOSC or HPOSC clk (use HPOSC when HPOSC_MODE_EN = 1) 2h = Low frequency RCOSC 3h = Low frequency XOSC |
| 1 | RESERVED | R | 0h | Reserved |
| 0 | SCLK_HF_SRC_SEL | R/W | 0h | Source select for sclk_hf.
0h = High frequency RCOSC clock 1h = High frequency XOSC or HPOSC clk (use HPOSC when HPOSC_MODE_EN = 1 |
CTL1 is shown in Figure 8-8 and described in Table 8-11.
Return to the Summary Table.
Control 1
This register contains OSC_DIG configuration
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | RCOSCHFCTRIMFRACT | RCOSCHFCTRIMFRACT_EN | RESERVED | ||||
| R-0h | R/W-0h | R/W-0h | R-0h | ||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | XOSC_HF_FAST_START | ||||||
| R-0h | R/W-0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-23 | RESERVED | R | 0h | Reserved |
| 22-18 | RCOSCHFCTRIMFRACT | R/W | 0h | Internal. Only to be used through TI provided API. |
| 17 | RCOSCHFCTRIMFRACT_EN | R/W | 0h | Internal. Only to be used through TI provided API. |
| 16-2 | RESERVED | R | 0h | Reserved |
| 1-0 | XOSC_HF_FAST_START | R/W | 0h | Internal. Only to be used through TI provided API. |
RADCEXTCFG is shown in Figure 8-9 and described in Table 8-12.
Return to the Summary Table.
RADC External Configuration
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| HPM_IBIAS_WAIT_CNT | |||||||
| R/W-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| HPM_IBIAS_WAIT_CNT | LPM_IBIAS_WAIT_CNT | ||||||
| R/W-0h | R/W-0h | ||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| IDAC_STEP | RADC_DAC_TH | ||||||
| R/W-0h | R/W-0h | ||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RADC_DAC_TH | RADC_MODE_IS_SAR | RESERVED | |||||
| R/W-0h | R/W-0h | R-0h | |||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-22 | HPM_IBIAS_WAIT_CNT | R/W | 0h | Internal. Only to be used through TI provided API. |
| 21-16 | LPM_IBIAS_WAIT_CNT | R/W | 0h | Internal. Only to be used through TI provided API. |
| 15-12 | IDAC_STEP | R/W | 0h | Internal. Only to be used through TI provided API. |
| 11-6 | RADC_DAC_TH | R/W | 0h | Internal. Only to be used through TI provided API. |
| 5 | RADC_MODE_IS_SAR | R/W | 0h | Internal. Only to be used through TI provided API. |
| 4-0 | RESERVED | R | 0h | Reserved |
AMPCOMPCTL is shown in Figure 8-10 and described in Table 8-13.
Return to the Summary Table.
Amplitude Compensation Control
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | AMPCOMP_REQ_MODE | AMPCOMP_FSM_UPDATE_RATE | AMPCOMP_SW_CTRL | AMPCOMP_SW_EN | RESERVED | ||
| R-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R-0h | ||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| IBIAS_OFFSET | IBIAS_INIT | ||||||
| R/W-0h | R/W-0h | ||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| LPM_IBIAS_WAIT_CNT_FINAL | |||||||
| R/W-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| CAP_STEP | IBIASCAP_HPTOLP_OL_CNT | ||||||
| R/W-0h | R/W-0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31 | RESERVED | R | 0h | Reserved |
| 30 | AMPCOMP_REQ_MODE | R/W | 0h | Internal. Only to be used through TI provided API. |
| 29-28 | AMPCOMP_FSM_UPDATE_RATE | R/W | 0h | Internal. Only to be used through TI provided API. |
| 27 | AMPCOMP_SW_CTRL | R/W | 0h | Internal. Only to be used through TI provided API. |
| 26 | AMPCOMP_SW_EN | R/W | 0h | Internal. Only to be used through TI provided API. |
| 25-24 | RESERVED | R | 0h | Reserved |
| 23-20 | IBIAS_OFFSET | R/W | 0h | Internal. Only to be used through TI provided API. |
| 19-16 | IBIAS_INIT | R/W | 0h | Internal. Only to be used through TI provided API. |
| 15-8 | LPM_IBIAS_WAIT_CNT_FINAL | R/W | 0h | Internal. Only to be used through TI provided API. |
| 7-4 | CAP_STEP | R/W | 0h | Internal. Only to be used through TI provided API. |
| 3-0 | IBIASCAP_HPTOLP_OL_CNT | R/W | 0h | Internal. Only to be used through TI provided API. |
AMPCOMPTH1 is shown in Figure 8-11 and described in Table 8-14.
Return to the Summary Table.
Amplitude Compensation Threshold 1
This register contains threshold values for amplitude compensation algorithm
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| HPMRAMP3_LTH | RESERVED | ||||||
| R/W-0h | R-0h | ||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| HPMRAMP3_HTH | IBIASCAP_LPTOHP_OL_CNT | ||||||
| R/W-0h | R/W-0h | ||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| IBIASCAP_LPTOHP_OL_CNT | HPMRAMP1_TH | ||||||
| R/W-0h | R/W-0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-24 | RESERVED | R | 0h | Reserved |
| 23-18 | HPMRAMP3_LTH | R/W | 0h | Internal. Only to be used through TI provided API. |
| 17-16 | RESERVED | R | 0h | Reserved |
| 15-10 | HPMRAMP3_HTH | R/W | 0h | Internal. Only to be used through TI provided API. |
| 9-6 | IBIASCAP_LPTOHP_OL_CNT | R/W | 0h | Internal. Only to be used through TI provided API. |
| 5-0 | HPMRAMP1_TH | R/W | 0h | Internal. Only to be used through TI provided API. |
AMPCOMPTH2 is shown in Figure 8-12 and described in Table 8-15.
Return to the Summary Table.
Amplitude Compensation Threshold 2
This register contains threshold values for amplitude compensation algorithm.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| LPMUPDATE_LTH | RESERVED | ||||||
| R/W-0h | R-0h | ||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| LPMUPDATE_HTH | RESERVED | ||||||
| R/W-0h | R-0h | ||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| ADC_COMP_AMPTH_LPM | RESERVED | ||||||
| R/W-0h | R-0h | ||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| ADC_COMP_AMPTH_HPM | RESERVED | ||||||
| R/W-0h | R-0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-26 | LPMUPDATE_LTH | R/W | 0h | Internal. Only to be used through TI provided API. |
| 25-24 | RESERVED | R | 0h | Reserved |
| 23-18 | LPMUPDATE_HTH | R/W | 0h | Internal. Only to be used through TI provided API. |
| 17-16 | RESERVED | R | 0h | Reserved |
| 15-10 | ADC_COMP_AMPTH_LPM | R/W | 0h | Internal. Only to be used through TI provided API. |
| 9-8 | RESERVED | R | 0h | Reserved |
| 7-2 | ADC_COMP_AMPTH_HPM | R/W | 0h | Internal. Only to be used through TI provided API. |
| 1-0 | RESERVED | R | 0h | Reserved |
ANABYPASSVAL1 is shown in Figure 8-13 and described in Table 8-16.
Return to the Summary Table.
Analog Bypass Values 1
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | XOSC_HF_ROW_Q12 | ||||||
| R-0h | R/W-0h | ||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| XOSC_HF_COLUMN_Q12 | |||||||
| R/W-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| XOSC_HF_COLUMN_Q12 | |||||||
| R/W-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-20 | RESERVED | R | 0h | Reserved |
| 19-16 | XOSC_HF_ROW_Q12 | R/W | 0h | Internal. Only to be used through TI provided API. |
| 15-0 | XOSC_HF_COLUMN_Q12 | R/W | 0h | Internal. Only to be used through TI provided API. |
ANABYPASSVAL2 is shown in Figure 8-14 and described in Table 8-17.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||||||||||
| R-0h | |||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | XOSC_HF_IBIASTHERM | ||||||||||||||
| R-0h | R/W-0h | ||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-14 | RESERVED | R | 0h | Reserved |
| 13-0 | XOSC_HF_IBIASTHERM | R/W | 0h | Internal. Only to be used through TI provided API. |
ATESTCTL is shown in Figure 8-15 and described in Table 8-18.
Return to the Summary Table.
Analog Test Control
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| SCLK_LF_AUX_EN | RESERVED | ||||||
| R/W-0h | R-0h | ||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| TEST_RCOSCMF | ATEST_RCOSCMF | RESERVED | |||||
| R/W-0h | R/W-0h | R-0h | |||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | |||||||
| R-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31 | SCLK_LF_AUX_EN | R/W | 0h | Enable 32 kHz clock to AUX_COMPB. |
| 30-16 | RESERVED | R | 0h | Reserved |
| 15-14 | TEST_RCOSCMF | R/W | 0h | Test mode control for RCOSC_MF 0x0: test modes disabled 0x1: boosted bias current into self biased inverter 0x2: clock qualification disabled 0x3: boosted bias current into self biased inverter + clock qualification disabled |
| 13-12 | ATEST_RCOSCMF | R/W | 0h | ATEST control for RCOSC_MF 0x0: ATEST disabled 0x1: ATEST enabled, VDD_LOCAL connected, ATEST internal to **RCOSC_MF* enabled to send out 2MHz clock. 0x2: ATEST disabled 0x3: ATEST enabled, bias current connected, ATEST internal to **RCOSC_MF* enabled to send out 2MHz clock. |
| 11-0 | RESERVED | R | 0h | Reserved |
ADCDOUBLERNANOAMPCTL is shown in Figure 8-16 and described in Table 8-19.
Return to the Summary Table.
ADC Doubler Nanoamp Control
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | NANOAMP_BIAS_ENABLE | ||||||
| R-0h | R/W-0h | ||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| SPARE23 | RESERVED | ||||||
| R/W-0h | R-0h | ||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | ADC_SH_MODE_EN | ADC_SH_VBUF_EN | RESERVED | ADC_IREF_CTRL | |||
| R-0h | R/W-0h | R/W-0h | R-0h | R/W-0h | |||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-25 | RESERVED | R | 0h | Reserved |
| 24 | NANOAMP_BIAS_ENABLE | R/W | 0h | Internal. Only to be used through TI provided API. |
| 23 | SPARE23 | R/W | 0h | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior |
| 22-6 | RESERVED | R | 0h | Reserved |
| 5 | ADC_SH_MODE_EN | R/W | 0h | Internal. Only to be used through TI provided API. |
| 4 | ADC_SH_VBUF_EN | R/W | 0h | Internal. Only to be used through TI provided API. |
| 3-2 | RESERVED | R | 0h | Reserved |
| 1-0 | ADC_IREF_CTRL | R/W | 0h | Internal. Only to be used through TI provided API. |
XOSCHFCTL is shown in Figure 8-17 and described in Table 8-20.
Return to the Summary Table.
XOSCHF Control
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | TCXO_MODE_XOSC_HF_EN | TCXO_MODE | RESERVED | PEAK_DET_ITRIM | |||
| R-0h | R/W-0h | R/W-0h | R-0h | R/W-0h | |||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | BYPASS | RESERVED | HP_BUF_ITRIM | LP_BUF_ITRIM | |||
| R-0h | R/W-0h | R-0h | R/W-0h | R/W-0h | |||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-14 | RESERVED | R | 0h | Reserved |
| 13 | TCXO_MODE_XOSC_HF_EN | R/W | 0h | If this register is 1 when TCXO_MODE is 1, then the XOSC_HF is enabled, turning on the XOSC_HF bias current allowing a DC bias point to be provided to the clipped-sine wave clock signal on external input. |
| 12 | TCXO_MODE | R/W | 0h | If this register is 1 when BYPASS is 1, this will enable clock qualification on the TCXO clock on external input. This register has no effect when BYPASS is 0. |
| 11-10 | RESERVED | R | 0h | Reserved |
| 9-8 | PEAK_DET_ITRIM | R/W | 0h | Internal. Only to be used through TI provided API. |
| 7 | RESERVED | R | 0h | Reserved |
| 6 | BYPASS | R/W | 0h | Internal. Only to be used through TI provided API. |
| 5 | RESERVED | R | 0h | Reserved |
| 4-2 | HP_BUF_ITRIM | R/W | 0h | Internal. Only to be used through TI provided API. |
| 1-0 | LP_BUF_ITRIM | R/W | 0h | Internal. Only to be used through TI provided API. |
LFOSCCTL is shown in Figure 8-18 and described in Table 8-21.
Return to the Summary Table.
Low Frequency Oscillator Control
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| XOSCLF_REGULATOR_TRIM | XOSCLF_CMIRRWR_RATIO | RESERVED | |||||
| R/W-0h | R/W-0h | R-0h | |||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | RCOSCLF_RTUNE_TRIM | ||||||
| R-0h | R/W-0h | ||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RCOSCLF_CTUNE_TRIM | |||||||
| R/W-0h | |||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-24 | RESERVED | R | 0h | Reserved |
| 23-22 | XOSCLF_REGULATOR_TRIM | R/W | 0h | Internal. Only to be used through TI provided API. |
| 21-18 | XOSCLF_CMIRRWR_RATIO | R/W | 0h | Internal. Only to be used through TI provided API. |
| 17-10 | RESERVED | R | 0h | Reserved |
| 9-8 | RCOSCLF_RTUNE_TRIM | R/W | 0h | Internal. Only to be used through TI provided API. |
| 7-0 | RCOSCLF_CTUNE_TRIM | R/W | 0h | Internal. Only to be used through TI provided API. |
RCOSCHFCTL is shown in Figure 8-19 and described in Table 8-22.
Return to the Summary Table.
RCOSCHF Control
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||||||||||
| R-0h | |||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RCOSCHF_CTRIM | RESERVED | ||||||||||||||
| R/W-0h | R-0h | ||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-8 | RCOSCHF_CTRIM | R/W | 0h | Internal. Only to be used through TI provided API. |
| 7-0 | RESERVED | R | 0h | Reserved |
RCOSCMFCTL is shown in Figure 8-20 and described in Table 8-23.
Return to the Summary Table.
RCOSC_MF Control
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RCOSC_MF_CAP_ARRAY | RCOSC_MF_REG_SEL | ||||||
| R/W-0h | R/W-0h | ||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RCOSC_MF_RES_COARSE | RCOSC_MF_RES_FINE | RCOSC_MF_BIAS_ADJ | |||||
| R/W-0h | R/W-0h | R/W-0h | |||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-9 | RCOSC_MF_CAP_ARRAY | R/W | 0h | Adjust RCOSC_MF capacitor array. 0x0: nominal frequency, 0.625pF 0x40: highest frequency, 0.125pF 0x3F: lowest frequency, 1.125pF |
| 8 | RCOSC_MF_REG_SEL | R/W | 0h | Choose regulator type. 0: default 1: alternate |
| 7-6 | RCOSC_MF_RES_COARSE | R/W | 0h | Select coarse resistor for frequency adjustment. 0x0: 400kΩs, default 0x1: 300kΩs, min 0x2: 600kΩs, max 0x3: 500kΩs |
| 5-4 | RCOSC_MF_RES_FINE | R/W | 0h | Select fine resistor for frequency adjustment. 0x0: 11kΩs, minimum resistance, max freq 0x1: 13kΩs 0x2: 16kΩs 0x3: 20kΩs, max resistance, min freq |
| 3-0 | RCOSC_MF_BIAS_ADJ | R/W | 0h | Adjusts bias current to RCOSC_MF. 0x8 minimum current 0x0 default current 0x7 maximum current |
STAT0 is shown in Figure 8-21 and described in Table 8-24.
Return to the Summary Table.
Status 0
This register contains status signals from OSC_DIG
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | SCLK_LF_SRC | SCLK_HF_SRC | RESERVED | ||||
| R-0h | R-0h | R-0h | R-0h | ||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | RCOSC_HF_EN | RCOSC_LF_EN | XOSC_LF_EN | CLK_DCDC_RDY | CLK_DCDC_RDY_ACK | SCLK_HF_LOSS | SCLK_LF_LOSS |
| R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| XOSC_HF_EN | RESERVED | XB_48M_CLK_EN | RESERVED | XOSC_HF_LP_BUF_EN | XOSC_HF_HP_BUF_EN | RESERVED | ADC_THMET |
| R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| ADC_DATA_READY | ADC_DATA | PENDINGSCLKHFSWITCHING | |||||
| R-0h | R-0h | R-0h | |||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31 | RESERVED | R | 0h | Reserved |
| 30-29 | SCLK_LF_SRC | R | 0h | Indicates source for the sclk_lf
0h = Low frequency clock derived from High Frequency RCOSC 1h = Low frequency clock derived from High Frequency XOSC 2h = Low frequency RCOSC 3h = Low frequency XOSC |
| 28 | SCLK_HF_SRC | R | 0h | Indicates source for the sclk_hf
0h = High frequency RCOSC clock 1h = High frequency XOSC |
| 27-23 | RESERVED | R | 0h | Reserved |
| 22 | RCOSC_HF_EN | R | 0h | RCOSC_HF_EN |
| 21 | RCOSC_LF_EN | R | 0h | RCOSC_LF_EN |
| 20 | XOSC_LF_EN | R | 0h | XOSC_LF_EN |
| 19 | CLK_DCDC_RDY | R | 0h | CLK_DCDC_RDY |
| 18 | CLK_DCDC_RDY_ACK | R | 0h | CLK_DCDC_RDY_ACK |
| 17 | SCLK_HF_LOSS | R | 0h | Indicates sclk_hf is lost |
| 16 | SCLK_LF_LOSS | R | 0h | Indicates sclk_lf is lost |
| 15 | XOSC_HF_EN | R | 0h | Indicates that XOSC_HF is enabled. |
| 14 | RESERVED | R | 0h | Reserved |
| 13 | XB_48M_CLK_EN | R | 0h | Indicates that the 48MHz clock from the DOUBLER is enabled. It will be enabled if 24 or 48 MHz crystal is used (enabled in doubler bypass for the 48MHz crystal). |
| 12 | RESERVED | R | 0h | Reserved |
| 11 | XOSC_HF_LP_BUF_EN | R | 0h | XOSC_HF_LP_BUF_EN |
| 10 | XOSC_HF_HP_BUF_EN | R | 0h | XOSC_HF_HP_BUF_EN |
| 9 | RESERVED | R | 0h | Reserved |
| 8 | ADC_THMET | R | 0h | ADC_THMET |
| 7 | ADC_DATA_READY | R | 0h | indicates when adc_data is ready. |
| 6-1 | ADC_DATA | R | 0h | adc_data |
| 0 | PENDINGSCLKHFSWITCHING | R | 0h | Indicates when SCLK_HF clock source is ready to be switched |
STAT1 is shown in Figure 8-22 and described in Table 8-25.
Return to the Summary Table.
Status 1
This register contains status signals from OSC_DIG
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RAMPSTATE | HPM_UPDATE_AMP | ||||||
| R-0h | R-0h | ||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| HPM_UPDATE_AMP | LPM_UPDATE_AMP | ||||||
| R-0h | R-0h | ||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| FORCE_RCOSC_HF | SCLK_HF_EN | SCLK_MF_EN | ACLK_ADC_EN | ACLK_TDC_EN | ACLK_REF_EN | CLK_CHP_EN | CLK_DCDC_EN |
| R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| SCLK_HF_GOOD | SCLK_MF_GOOD | SCLK_LF_GOOD | ACLK_ADC_GOOD | ACLK_TDC_GOOD | ACLK_REF_GOOD | CLK_CHP_GOOD | CLK_DCDC_GOOD |
| R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-28 | RAMPSTATE | R | 0h | AMPCOMP FSM State
0h = RESET 1h = INITIALIZATION 2h = HPM_RAMP1 3h = HPM_RAMP2 4h = HPM_RAMP3 5h = HPM_UPDATE 6h = IDAC_INCREMENT 7h = IBIAS_CAP_UPDATE 8h = IBIAS_DECREMENT_WITH_MEASURE 9h = LPM_UPDATE Ah = IBIAS_INCREMENT Bh = IDAC_DECREMENT_WITH_MEASURE Ch = DUMMY_TO_INIT_1 Dh = FAST_START Eh = FAST_START_SETTLE |
| 27-22 | HPM_UPDATE_AMP | R | 0h | XOSC_HF amplitude during HPM_UPDATE state. When amplitude compensation of XOSC_HF is enabled in high performance mode, this value is the amplitude of the crystal oscillations measured by the on-chip oscillator ADC, divided by 15 mV. For example, a value of 0x20 would indicate that the amplitude of the crystal is approximately 480 mV. To enable amplitude compensation, AON_WUC OSCCFG must be set to a non-zero value. |
| 21-16 | LPM_UPDATE_AMP | R | 0h | XOSC_HF amplitude during LPM_UPDATE state When amplitude compensation of XOSC_HF is enabled in low power mode, this value is the amplitude of the crystal oscillations measured by the on-chip oscillator ADC, divided by 15 mV. For example, a value of 0x20 would indicate that the amplitude of the crystal is approximately 480 mV. To enable amplitude compensation, AON_WUC OSCCFG must be set to a non-zero value. |
| 15 | FORCE_RCOSC_HF | R | 0h | force_rcosc_hf |
| 14 | SCLK_HF_EN | R | 0h | SCLK_HF_EN |
| 13 | SCLK_MF_EN | R | 0h | SCLK_MF_EN |
| 12 | ACLK_ADC_EN | R | 0h | ACLK_ADC_EN |
| 11 | ACLK_TDC_EN | R | 0h | ACLK_TDC_EN |
| 10 | ACLK_REF_EN | R | 0h | ACLK_REF_EN |
| 9 | CLK_CHP_EN | R | 0h | CLK_CHP_EN |
| 8 | CLK_DCDC_EN | R | 0h | CLK_DCDC_EN |
| 7 | SCLK_HF_GOOD | R | 0h | SCLK_HF_GOOD |
| 6 | SCLK_MF_GOOD | R | 0h | SCLK_MF_GOOD |
| 5 | SCLK_LF_GOOD | R | 0h | SCLK_LF_GOOD |
| 4 | ACLK_ADC_GOOD | R | 0h | ACLK_ADC_GOOD |
| 3 | ACLK_TDC_GOOD | R | 0h | ACLK_TDC_GOOD |
| 2 | ACLK_REF_GOOD | R | 0h | ACLK_REF_GOOD. |
| 1 | CLK_CHP_GOOD | R | 0h | CLK_CHP_GOOD |
| 0 | CLK_DCDC_GOOD | R | 0h | CLK_DCDC_GOOD |
STAT2 is shown in Figure 8-23 and described in Table 8-26.
Return to the Summary Table.
Status 2
This register contains status signals from AMPCOMP FSM
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| ADC_DCBIAS | HPM_RAMP1_THMET | HPM_RAMP2_THMET | |||||
| R-0h | R-0h | R-0h | |||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| HPM_RAMP3_THMET | RESERVED | ||||||
| R-0h | R-0h | ||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RAMPSTATE | RESERVED | ||||||
| R-0h | R-0h | ||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | AMPCOMP_REQ | XOSC_HF_AMPGOOD | XOSC_HF_FREQGOOD | XOSC_HF_RF_FREQGOOD | |||
| R-0h | R-0h | R-0h | R-0h | R-0h | |||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-26 | ADC_DCBIAS | R | 0h | DC Bias read by RADC during SAR mode The value is an unsigned integer. It is used for debug only. |
| 25 | HPM_RAMP1_THMET | R | 0h | Indication of threshold is met for hpm_ramp1 |
| 24 | HPM_RAMP2_THMET | R | 0h | Indication of threshold is met for hpm_ramp2 |
| 23 | HPM_RAMP3_THMET | R | 0h | Indication of threshold is met for hpm_ramp3 |
| 22-16 | RESERVED | R | 0h | Reserved |
| 15-12 | RAMPSTATE | R | 0h | xosc_hf amplitude compensation FSM This is identical to STAT1.RAMPSTATE. See that description for encoding. |
| 11-4 | RESERVED | R | 0h | Reserved |
| 3 | AMPCOMP_REQ | R | 0h | ampcomp_req |
| 2 | XOSC_HF_AMPGOOD | R | 0h | amplitude of xosc_hf is within the required threshold (set by DDI). Not used for anything just for debug/status |
| 1 | XOSC_HF_FREQGOOD | R | 0h | frequency of xosc_hf is good to use for the digital clocks |
| 0 | XOSC_HF_RF_FREQGOOD | R | 0h | frequency of xosc_hf is within +/- 20 ppm and xosc_hf is good for radio operations. Used for SW to start synthesizer. |