SPRAD28 October 2022 AM2431 , AM2432 , AM2434 , AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM263P2-Q1 , AM263P4 , AM263P4-Q1 , AM26C31-EP , AM26C31M , AM26C32-EP , AM26C32C , AM26C32M , AM26LS31M , AM26LS32AM , AM26LS33A-SP , AM26LS33AM , AM26LV31E-EP , AM26LV32E-EP , AM26S10 , AM2732 , AM2732-Q1
To open the Memory Browser view: View → Memory Browser
The Memory Browser view is another integral part of the debugger that shows the contents of the target memory starting at a specified address and with various data formatting features.
To use it, enter an address in the Address Text box at the top of the view. The contents of a selected memory location can be edited by double-clicking the value.
It features multiple viewing formats and types:
Chars, integers (signed/unsigned), floats, multiple hexadecimal data sizes (8 through 64-bits).
Additional capabilities include: