SPRAD28 October 2022 AM2431 , AM2432 , AM2434 , AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM26C31 , AM26C31-EP , AM26C31C , AM26C31I , AM26C31M , AM26C32 , AM26C32-EP , AM26C32C , AM26C32M , AM26LS31 , AM26LS31M , AM26LS32A , AM26LS32AC , AM26LS32AM , AM26LS33A , AM26LS33A-SP , AM26LS33AM , AM26LV31 , AM26LV31E , AM26LV31E-EP , AM26LV32 , AM26LV32E , AM26LV32E-EP , AM26S10 , AM2732 , AM2732-Q1
The SDK provides two versions of libs: "Debug" and "Release". The "Debug" version is built with optimization disabled, while the "Release" version is built with optimization enabled. The recommendation is to use the "Debug" version of an SDK lib when debugging.
The SDK libs follow the naming convention: "{library name}.{device}.{core}.{compiler}.{version}.lib"
For example, "drivers.am243x.m4f.ti-arm-clang.release.lib" implies the following:
The libraries that are linked to your project can be configured in the project properties under Build > Arm Linker > File Search Path.