SPRACE5A May 2019 – May 2021 F28377D-SEP , F29H850DM , F29H850TU , F29H859TU-Q1 , F29P329SM-Q1 , F29P589DM-Q1 , F29P589DU-Q1 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28076 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28384D , TMS320F28384S , TMS320F28386D , TMS320F28386S , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
In this section, the usage of the various bit-fields in the CANBTR register is illustrated.
The formula for bit-rate is:

Where BRP is the value of (BRPreg + 1) and Bit-time = (TSEG1reg + 1) + (TSEG2reg + 1) + 1
In the above equations BRPreg , TESG1reg and TSEG2reg represent the actual values written in the corresponding fields in the CANBTR register. The parameters TSEG1reg, TSEG2reg, SJWreg, and BRPreg are automatically enhanced by 1 when the CAN module accesses these parameters. If the BRPE field is used, it should be concatenated with the BRP field.
Example 1
Assume the following parameters are desired with a CAN module clock of 200 MHz:
Bit-rate = 500 kbps, SJW = 4, TSEG1 = 9 & TSEG2 = 6.
This is achieved by writing a value of 0x000058D8 in the CANBTR register. Here, TSEG1reg = 8, TSEG2reg = 5, SJWreg = 3, and BRPreg = 24
Effective BRP value = (BRPreg + 1) = 25
Effective TSEG1 value = (TSEG1reg + 1) = 9
Effective TSEG2 value = (TSEG2reg + 1) = 6
Effective SJW value = (SJWreg + 1) = 4
Bit-time = (TSEG1reg + 1) + (TSEG2reg + 1) + 1 = 16
Plugging these numbers into the bit-rate equation:

Example 2
Assume the following parameters are desired with a CAN module clock of 200 MHz:
Bit-rate = 50 kbps, SJW = 4, TSEG1 = 9 & TSEG2 = 6.
This is achieved by writing a value of 0x000358F9 in the CANBTR register. Here, TSEG1reg = 8, TSEG2reg = 5, SJWreg = 3, BRPE = 11b , BRP = 111001b. Effective BRPreg = 11111001b (249). Note that BRPE field is concatenated with the BRP field.
Effective BRP value = (BRPreg + 1) = 250
Effective TSEG1 value = (TSEG1reg + 1) = 9
Effective TSEG2 value = (TSEG2reg + 1) = 6
Effective SJW value = (SJWreg + 1) = 4
Bit-time = (TSEG1reg + 1) + (TSEG2reg + 1) + 1 = 16
Plugging these numbers into the bit-rate equation: