SLUUCD5B January 2023 – June 2026 BQ27427
The wait command indicates that the host waits a minimum of the given number of milliseconds before continuing to the next row of the FlashStream file. A wait command is typically used to allow the fuel gauge processor to complete a process before proceeding to the next command in the file.
For example, the following:
X: 200Indicates that the I2C primary must wait at least 200 ms before continuing.