SLUUCD5B January 2023 – June 2026 BQ27427
Temperature information for the fuel gauge can be configured from three separate sources:
The OpConfig [TEMPS] bits can be used to select the source, as shown below:
| OpConfig [TEMPS] | Temperature Source |
|---|---|
| 00 | Internal Temperature Sensor is used as Temperature Source. |
| 01 | External Thermistor is used as Temperature Source. |
| 10 | Host written Temperature is used as Temperature Source. |
Regardless of which sensor is used for measurement, the system processor can request the current battery temperature being used by the algorithm by calling the Temperature() function.