SBAK043 April 2026 DAC39RF10-SP , DAC39RFS10-SP
| Feature | Radiation Hardening |
|---|---|
| Writable SPI registers (excluding write-to-clear registers) | Implemented with upset-immune flip-flops. Radiation will not alter their state. |
| Read-only SPI registers that return constant values | Radiation will not alter their state (for example, CHIP_TYPE, CHIP_ID, CHIP_VERSION, VENDOR_ID). |
| Read-only SPI status registers associated with JESD204C physical or link layers (excluding write-to-clear registers) | The value returned may be affected by radiation (SYSREF_POS, LINK_UP, JSYNC_STATE, PLL_LOCKED, LANE_ARR, FIFO_STATUS, JCAP_STATUS, JCAP, BER_CNT, LANE_EQS, ESDONE, ESVO_S, ECOUNT, RXDMUX, CDRPHASE, RXCSA_S). |
| FUSE_DONE register | FUSE_DONE is upset-immune. |
| OCSTS register | Once the PHY is initialized and offset calibration is completed, OCSTS returns offset values that are upset-immune. However, an upset can cause a PHY PLL to lose lock which can re-trigger the offset calibration process, generating new offset calibration values. |
| Sticky SPI status registers (write-to-clear) | These bits get set when certain events occur in upset-vulnerable logic. An upset can cause the event to occur and set the sticky bit. An upset may also prevent an event from setting the sticky bit, however this is unlikely as the window of time that this can occur is very small. Once the sticky bit is set, an upset will not clear it (the flop that is read by SPI is upset immune).Examples: LANE_ERR, PLL_LOCK_LOST, SYS_ALM, REALIGNED, CLK_REALIGNED |
| JESD204C receiver | The JESD204C receiver is not upset-immune, but is designed to be free from functional interrupts (can recover automatically from upsets). See JESD204C Reliability section below. |
| Interpolation filters (DUC and DES2X filters) | The interpolation filters are not upset-immune and will generate glitches when upset. They do not suffer from functional interrupts. |
| NCOs in DUCs | See NCO Reliability section below. |
| Temperature sensor | The ADC inside the temperature sensor is not upset-immune. To improve reliability, it is recommended that TS_TEMP be read 3 or more times and the median value computed. |