This strategy uses a periodic
reference signal to correct any upsets in the NCO accumulator. This strategy is
appropriate for phased-array systems or other systems where the NCO phase must
remain coherent with other system components, including other DAC39RF10-SP
parts.
- Program NCO_AR = 1 to configure
the accumulator to be reset on every synchronization event.
- Configure the NCO to use SYSREF
as the synchronization source (NCO_SYNC_SRC = 2). Program SPI_SYNC = 1.
- Verify the SYSREF generator is
configured for continuous/periodic output.
- Since the accumulator will be
reset periodically, you must ensure that the programmed NCO frequency is an
integer multiple of the SYSREF frequency. Consider the frequency raster that
your system requires when you choose the SYSREF frequency.
- If you cannot choose a SYSREF
frequency that satisfies your frequency raster and is also a sub-harmonic of the
multi-frame/EMB frequency, then you can use the LSB of the JESD204C data stream
to periodically synchronize the NCO. Use NCO_SYNC_SRC = 3, and provide a
periodic reference signal on the LSB of the I samples for DUC0.
- If any NCO accumulator or
internal frequency register is upset, it will be restored on the next
synchronization event.