ZHCSQ47 March 2022 LP8764-Q1
PRODUCTION DATA
Description: Delay the execution by a specified time
Assembly command: DELAY_IMM <Delay>
Delay = delay time in ns, µs, ms, or s. If no unit is entered, this field must be an integer value between 0-63. Delay value is be rounded to the nearest achievable time based on the current step size. Current step size is based on the default NVM setting or a SET_DELAY value from a previous command in the same sequence. Assembler reports an error if the step size is too large or too small to meet the delay.
Examples: