ZHCSDS3C May 2015 – April 2018 ADS52J90
PRODUCTION DATA.
By default, each serializer takes in one SERIAL_IN word and performs a parallel-to-serial conversion. This mode is referred to as the 1X data rate mode. In the 1X data rate mode, all 16 LVDS pairs are active and each pair corresponds to the data coming out of one ADC. In the 2X data rate mode (set using the LVDS_RATE_2X bit), the data from a pair of ADCs (two SERIAL_IN words) is packed into the same serial stream. In 2X mode, half the LVDS pairs are idle and can be powered down. The 2X data rate mode causes the LVDS interface to run at twice the rate but results in power saving. See the Timing Requirements: Signal Chain table for speed restrictions when using the 1X and 2X data rate modes.
The LVDS interface is a clock-data-frame (CDF) format, and has a frame clock and a high-speed bit clock in addition to the serial data lines.
The frequency of the bit clock with respect to the conversion clock frequency depends on the serialization factor (set using the SER_DATA_RATE bits), as shown in Table 10. Note that the serialized data are meant to be captured on both the rising and falling edges of the bit clock. Thus, the serialized data rate is twice the bit clock frequency.
| SERIALIZATION FACTOR | DATA RATE MODE | BIT CLOCK RATE
(fB in Terms of fC) |
BIT CLOCK RATE (fB in Terms of fS) | ||
|---|---|---|---|---|---|
| 16-INPUT MODE | 32-INPUT MODE | 8-INPUT MODE | |||
| 10 | 1X | 5 × fC | 5 × fS | 5 × fS | 2.5 × fS |
| 2X | 10 × fC | 10 × fS | 10 × fS | 5 × fS | |
| 12 | 1X | 6 × fC | 6 × fS | 6 × fS | 3 × fS |
| 2X | 12 × fC | 12 × fS | 12 × fS | 6 × fS | |
| 14 | 1X | 7 × fC | 7 × fS | 7 × fS | 3.5 × fS |
| 2X | 14 × fC | 14 × fS | 14 × fS | 7 × fS | |
| 16 | 1X | 8 × fC | 8 × fS | 8 × fS | 4 × fS |
| 2X | 16 × fC | 16 × fS | 16 × fS | 8 × fS | |
The relationship of the frame clock frequency to the conversion clock frequency for the three input modes is as shown in Table 11. The relationship of the frame clock frequency to the system clock (and conversion clock) frequencies is the same between the 1X and 2X data rate modes.
| ANALOG INPUT MODE
(Number of Channels) |
FRAME CLOCK RATE
(fF in Terms of fC) |
FRAME CLOCK RATE
(fF in Terms of fS) |
DATA RATE MODES SUPPORTED |
|---|---|---|---|
| 16 | fC | fS | 1X, 2X |
| 32 | 0.5 × fC | 0.5 × fS | 1X |
| 8 | fC | 0.5 × fS | 1X, 2X |
The serialization schemes for the various modes are illustrated in Figure 64 to Figure 68. Note that although the signals marked ADCx Conversion in Figure 64 to Figure 68 represent a multi-bit digital word, the SERIAL_OUTx signals are actually serialized representations of the correspondingly colored signals. For example, the blue-colored section in the SERIAL_OUT1 signal in Figure 64 contains the serial stream of data that originated from the word corresponding to ADC1o.
Figure 65. ADC to Output Mapping in 8-Input, 1X Mode in LVDS Interface Mode
Figure 66. ADC to Output Mapping in 16-Input, 2X Mode in LVDS Interface Mode
Figure 67. ADC to Output Mapping in 8-Input, 2X Mode in LVDS Interface Mode
Figure 68. ADC to Output Mapping in 32-Input, 1X Mode in LVDS Interface Mode
The mapping of the subsequent-numbered ADC signals to subsequent-numbered SERIAL_OUT signals follows the same pattern as indicated previously.
The serialized stream in SERIAL_OUT is a serialized representation of SERIAL_IN, which is the input word coming into the serializer. By default, serialization is done LSB-first. By setting the MSB_FIRST bit, serialization can be set to MSB-first.
The alignment of the frame clock, bit clock, and the serialized output data is illustrated in Figure 1 for 16-input mode where the serialization factor is set to 12 bit, serialization is LSB-first, and the data rate is set to 1X mode.
Another case is shown in Figure 69 for 16-input mode. Here, the serialization factor is set to 14 bit, serialization is MSB-first, and the data rate is set to 2X mode.
Figure 69. LVDS Output Signals Timing Diagram in 16-Input Mode with
The serialized signals come out on the DOUT pins as indicated in Table 12. The buffers marked Idle can be powered down using the appropriate register bits to save power.
| LVDS OUTPUT PIN (DOUT) | OUTPUT SIGNAL | |
|---|---|---|
| 1X DATA RATE MODE | 2X DATA RATE MODE | |
| DOUT1 | SERIAL_OUT1 | SERIAL_OUT1 |
| DOUT2 | SERIAL_OUT2 | SERIAL_OUT3 |
| DOUT3 | SERIAL_OUT3 | SERIAL_OUT5 |
| DOUT4 | SERIAL_OUT4 | SERIAL_OUT7 |
| DOUT5 | SERIAL_OUT5 | Idle |
| DOUT6 | SERIAL_OUT6 | Idle |
| DOUT7 | SERIAL_OUT7 | Idle |
| DOUT8 | SERIAL_OUT8 | Idle |
| DOUT9 | SERIAL_OUT9 | SERIAL_OUT9 |
| DOUT10 | SERIAL_OUT10 | SERIAL_OUT11 |
| DOUT11 | SERIAL_OUT11 | SERIAL_OUT13 |
| DOUT12 | SERIAL_OUT12 | SERIAL_OUT15 |
| DOUT13 | SERIAL_OUT13 | Idle |
| DOUT14 | SERIAL_OUT14 | Idle |
| DOUT15 | SERIAL_OUT15 | Idle |
| DOUT16 | SERIAL_OUT16 | Idle |