SWRU580 April   2021 CC2564C , CC2564MODA , CC2564MODN

 

  1.   Trademarks
  2. 1 Introduction
  3. 2 A2DP (AUD) Demo Guide
    1. 2.1 Demo Overview
    2. 2.2 Demo Application
    3. 2.3 Application Commands
  4. 3 A3DP Sink Demo Guide
    1. 3.1 Demo Overview
    2. 3.2 Demo Application
    3. 3.3 Sink Reference Board Demo Application
    4. 3.4 Multiple Source Demo
    5. 3.5 Application Commands
  5. 4 A3DP Source Demo Guide
    1. 4.1 Demo Overview
    2. 4.2 Demo Application
    3. 4.3 Application Commands
  6. 5 HFP Demo Guide
    1. 5.1 Demo Overview
    2. 5.2 Demo Application
    3. 5.3 Application Commands
  7. 6 HFP Audio Gateway Demo Guide
    1. 6.1 Demo Overview
    2. 6.2 Demo Application
    3. 6.3 Application Commands
  8. 7 HID Demo Guide
    1. 7.1 Demo Overview
    2. 7.2 Demo Application
    3. 7.3 Application Commands
  9. 8 HSP Demo Guide
    1. 8.1 Demo Overview
    2. 8.2 Demo Application
    3. 8.3 Application Command
  10. 9 Map Demo Guide
    1. 9.1 Demo Overview
    2. 9.2 Demo Application
    3. 9.3 Application Command
  11. 10PBAP Demo Guide
    1. 10.1 Demo Overview
    2. 10.2 Demo Application
    3. 10.3 Application Commands
  12. 11SPP Demo Guide
    1. 11.1 Demo Overview
    2. 11.2 Demo Application
    3. 11.3 Application Commands
  13. 12SPPLE Demo Guide
    1. 12.1 Demo Overview
    2. 12.2 Demo Application
    3. 12.3 Demonstrating SPP LE on an iOS Device with the LightBlue App
    4. 12.4 Demonstrating SPP LE on an iOS Device with the SPPLE Transfer App - LEGACY
    5. 12.5 SPP Demo
    6. 12.6 Application Commands
  14. 13SPPDMMulti Demo Guide
    1. 13.1 Demo Overview
    2. 13.2 Demo Application
    3. 13.3 Application Commands
  15. 14ANP Demo Guide
    1. 14.1 Demo Overview
    2. 14.2 Demo Application
    3. 14.3 Application Commands
  16. 15HFP Demo Guide
    1. 15.1 Demo Overview
    2. 15.2 Demo Application
    3. 15.3 Application Commands
  17. 16HTP Demo Guide
    1. 16.1 Demo Overview
    2. 16.2 Demo Application
    3. 16.3 Application Commands
  18. 17PASP Demo Guide
    1. 17.1 Demo Overview
    2. 17.2 Demo Application
    3. 17.3 Application Commands
  19. 18HOGP Demo Guide
    1. 18.1 Demo Overview
    2. 18.2 Demo Application
    3. 18.3 Application Commands
  20. 19PXP Demo Guide
    1. 19.1 Demo Overview
    2. 19.2 Demo Application
    3. 19.3 Applications Commands
  21. 20FMP Demo Guide
    1. 20.1 Demo Overview
    2. 20.2 Demo Application
    3. 20.3 Application Commands
  22. 21CSCP Demo Guide
    1. 21.1 Demo Overview
    2. 21.2 Demo Application
    3. 21.3 Application Commands
  23. 22Revision History

Application Commands

Generic Access Profile Commands
Note: Reference the appendix for all Generic Access Profile Commands
BR/EDR Commands

For BR/EDR Commands refer to the document SPP Profile sections Generic Access Profile Commands and Serial Port Profile Commands.

GAPLE Commands

The Generic Access Profile defines standard procedures related to the discovery and connection of Bluetooth devices. It defines modes of operation that are generic to all devices and allows for procedures which use those modes to decide how a device can be interacted with by other Bluetooth devices. Discoverability, Connectability, Pairability, Bondable Modes, and Security Modes can all be changed using Generic Access Profile procedures. All of these modes affect the interaction two devices may have with one another. GAP also defines the procedures for how bond two Bluetooth devices.


SetDiscoverabilityMode

Description

The SetDiscoverabilityMode command is responsible for setting the Discoverability Mode of the local device. This command returns zero on successful execution and a negative value on all errors. The Discoverability Mode in LE is only applicable when advertising, if a device is not advertising it is not discoverable. The value set by this command will be used as a parameter in the command AdvertiseLE.

Parameters

This command requires only one parameter which is an integer value that represents a Discoverability Mode. This value must be specified as 0 (for Non-Discoverable Mode), 1 (for Limited Discoverable Mode), or 2 (for General Discoverable Mode).

Command Call Examples

"SetDiscoverabilityMode 0" Attempts to change the Discoverability Mode of the Local Device to Non-Discoverable. "SetDiscoverabilityMode 1" Attempts to change the Discoverability Mode of the Local Device to Limited Discoverable. "SetDiscoverabilityMode 2" Attempts to change the Discoverability Mode of the Local Device to General Discoverable.

Possible Return Values

(0) Successfully Set Discoverability Mode Parameter

(-6) INVALID_PARAMETERS_ERROR

(-8) INVALID_STACK_ID_ERROR


SetConnectabilityMode

Description

The SetConnectabilityMode command is responsible for setting the Connectability Mode of the local device. This command returns zero on successful execution and a negative value on all errors. The Connectability Mode in LE is only applicable when advertising, if a device is not advertising it is not connectable. The value set by this command will be used as a parameter in the command AdvertiseLE.

Parameters

This command requires only one parameter which is an integer value that represents a Connectability Mode. This value must be specified as 0 (for Non-Connectable) or 1 (for Connectable).

Command Call Examples

"SetConnectabilityMode 0" Attempts to set the Local Device’s Connectability Mode to Non-Connectable. "SetConnectabilityMode 1" Attempts to set the Local Device’s Connectability Mode to Connectable.

Possible Return Values

(0) Successfully Set Connectability Mode Parameter

(-6) INVALID_PARAMETERS_ERROR

(-8) INVALID_STACK_ID_ERROR


SetPairabilityMode

Description

The SetPairabilityMode command is responsible for setting the Pairability Mode of the local device. This command returns zero on successful execution and a negative value on all errors.

Parameters

This command requires only one parameter which is an integer value that represents a Pairability Mode. This value must be specified as 0 (for Non-Pairable), 1 (for Pairable) or 2(for Pairable with Secure Simple Pairing).

Command Call Examples

“SetPairabilityMode 0” Attempts to set the Local Device’s Pairability Mode to Non-Pairable. “SetPairabilityMode 1” Attempts to set the Local Device’s Pairability Mode to Pairable.

Possible Return Values

(0) Successfully Set Pairability Mode

(-4) FUNCTION_ERROR

(-6) INVALID_PARAMETERS_ERROR

(-8) INVALID_STACK_ID_ERROR

API Call

GAP_LE_Set_Pairability_Mode(BluetoothStackID, PairabilityMode);

API Prototype

int BTPSAPI GAP_LE_Set_Pairability_Mode(unsigned int BluetoothStackID, GAP_LE_Pairability_Mode_t PairableMode);

Description of API

This function is provided to allow the local host the ability to change the pairability mode used by the local host. This function will return zero if successful or a negative return error code if there was an error condition.


ChangePairingParameters

Description

The ChangePairingParameters command is responsible for changing the LE Pairing Parameters that are exchanged during the Pairing procedure. This command returns zero on successful execution and a negative value on all errors.

Parameters

This command requires five parameters which are the I/O Capability, the Bonding Type, the MITM Requirement, the SC Enable and the P256 debug mode.

The first parameter must be specified as 0 (for Display Only), 1 (for Display Yes/No), 2 (for Keyboard Only), 3 (for No Input/Output) or 4 (for Keyboard/Display).

The second parameter must be specified as 0 (for No Bonding) or 1 (for Bonding), when at least one of the devices is set to No Bonding, the LTK won't be stored.

The third parameter must be specified as 0 (for No MITM) or 1 (for MITM required).

The fourth parameter must be specified as 0 (for SC disabled) or 1 (for SC enabled), when using SC disable, legacy pairing procedure will take place.

The fifth parameter must be specified as 0 (for Debug Mode disabled) or 1 (for P256 debug mode enabled), Only when using SC pairing, P256 debug mode is relevant and when it is set, the values of the P256 private and public keys will be pre-defined according to the Bluetooth specification instead of random.

Command Call Examples

"ChangeSimplePairingParameters 3 0 0 0 0" Attempts to set the I/O Capability to No Input/Output, Bonding Type set to No Bonding, turns off MITM Protection, Disable secure connections and disable debug mode.

"ChangeSimplePairingParameters 2 0 1 1 0 " Attempts to set the I/O Capability to Keyboard Only, Bonding Type set to No Bonding, activates MITM Protection, Enabling secure connections and disable debug mode.

"ChangeSimplePairingParameters 1 1 1 1 1" Attempts to set the I/O Capability to Display Yes/No, Bonding Type set to Bonding, activates MITM Protection, Enabling secure connections and enabling debug mode.

Possible Return Values

(0) Successfully Set Pairability Mode

(-6) INVALID_PARAMETERS_ERROR

(-8) INVALID_STACK_ID_ERROR


AdvertiseLE

Description

The AdvertiseLE command is responsible for enabling LE Advertisements. This command returns zero on successful execution and a negative value on all errors.

Parameters

The only parameter necessary decides whether Advertising Reports are sent or are disabled. To Disable, use 0 as the first parameter, to enable, use 1 instead.

Command Call Examples

“AdvertiseLE 1” Attempts to enable Low Energy Advertising on the local Bluetooth device. “AdvertiseLE 0” Attempts to disable Low Energy Advertising on the local Bluetooth device.

Possible Return Values

(0) Successfully Set Pairability Mode

(-4) FUNCTION_ERROR

(-6) INVALID_PARAMETERS_ERROR

(-8) INVALID_STACK_ID_ERROR

(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID

(-1) BTPS_ERROR_INVALID_PARAMETER

(-56) BTPS_ERROR_GAP_NOT_INITIALIZED

(-104) BTPS_ERROR_LOCAL_CONTROLLER_DOES_NOT_SUPPORT_LE

(-57) BTPS_ERROR_DEVICE_HCI_ERROR

API Calls

Depending on the First Parameter Value

GAP_LE_Advertising_Disable(BluetoothStackID);

GAP_LE_Set_Advertising_Data(BluetoothStackID, (Advertisement_Data_Buffer.AdvertisingData.Advertising_Data[0] + 1), &(Advertisement_Data_Buffer.AdvertisingData));

GAP_LE_Set_Scan_Response_Data(BluetoothStackID, (Advertisement_Data_Buffer.ScanResponseData.Scan_Response_Data[0] + 1), &(Advertisement_Data_Buffer.ScanResponseData));

GAP_LE_Advertising_Enable(BluetoothStackID, TRUE, &AdvertisingParameters, &ConnectabilityParameters, GAP_LE_Event_Callback, 0);

API Prototypes

int BTPSAPI GAP_LE_Advertising_Disable(unsigned int BluetoothStackID);

int BTPSAPI GAP_LE_Set_Advertising_Data(unsigned int BluetoothStackID, unsigned int Length, Advertising_Data_t *Advertising_Data);

int BTPSAPI GAP_LE_Set_Scan_Response_Data(unsigned int BluetoothStackID, unsigned int Length, Scan_Response_Data_t *Scan_Response_Data);

int BTPSAPI GAP_LE_Set_Advertising_Data(unsigned int BluetoothStackID, unsigned int Length, Advertising_Data_t *Advertising_Data);

int BTPSAPI GAP_LE_Set_Advertising_Data(unsigned int BluetoothStackID, unsigned int Length, Advertising_Data_t *Advertising_Data);

Description of API

The GAP_LE_Advertising_Disable function is provided to allow the local host the ability to cancel (stop) an on-going advertising procedure. This function will return zero if successful or a negative return error code if there was an error condition. The GAP_LE_Set_Advertising_Data is provided to allow the local host the ability to set the advertising data that is used during the advertising procedure (started via the GAP_LE_Advertising_Enable function). This function will return zero if successful or a negative return error code if there was an error condition. The GAP_LE_Set_Scan_Response_Data function is provided to allow the local host the ability to set the advertising data that is used during the advertising procedure (started via the GAP_LE_Advertising_Enable function). This function will return zero if successful or a negative return error code if there was an error condition. The GAP_LE_Set_Advertising_Data function is provided to allow the local host the ability to set the advertising data that is used during the advertising procedure (started via the GAP_LE_Advertising_Enable function). This function will return zero if successful or a negative return error code if there was an error condition.


StartScanning

Description

The StartScanning command is responsible for starting an LE scan procedure. This command returns zero if successful and a negative value if an error occurred. This command calls the StartScan(unsigned int BluetoothStackID) function which performs the scan.

Parameters

It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome of the Scan.

Possible Return Values

(0) Successfully started the LE Scan Procedure

(-1) Bluetooth Stack ID is Invalid during the StartScan() call

(-4) FUNCTION_ERROR

(-8) INVALID_STACK_ID_ERROR

(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID

(-1) BTPS_ERROR_INVALID_PARAMETER

(-66) BTPS_ERROR_INSUFFICIENT_RESOURCES

(-105) BTPS_ERROR_SCAN_ACTIVE

(-56) BTPS_ERROR_GAP_NOT_INITIALIZED

(-104) BTPS_ERROR_LOCAL_CONTROLLER_DOES_NOT_SUPPORT_LE

(-57) BTPS_ERROR_DEVICE_HCI_ERROR

API Call

GAP_LE_Perform_Scan(BluetoothStackID, stActive, 10, 10, latPublic, fpNoFilter, TRUE, GAP_LE_Event_Callback, 0);

API Prototype

int BTPSAPI GAP_LE_Perform_Scan(unsigned int BluetoothStackID, GAP_LE_Scan_Type_t ScanType, unsigned int ScanInterval, unsigned int ScanWindow, GAP_LE_Address_Type_t LocalAddressType, GAP_LE_Filter_Policy_t FilterPolicy, Boolean_t FilterDuplicates, GAP_LE_Event_Callback_t GAP_LE_Event_Callback, unsigned long CallbackParameter);

Description of API

The GAP_LE_Perform_Scan function is provided to allow the local host the ability to begin an LE scanning procedure. This procedure is similar in concept to the inquiry procedure in Bluetooth BR/EDR in that it can be used to discover devices that have been instructed to advertise. This function will return zero if successful, or a negative return error code if there was an error condition.


StopScanning

Description

The StopScanning command is responsible for stopping an LE scan procedure. This command returns zero if successful and a negative value if an error occurred. This command calls the StopScan(unsigned int BluetoothStackID) function which performs the scan.

Parameters

It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome of disabling Scanning.

Possible Return Values

(0) Successfully stopped the LE Scan Procedure

(-1) Bluetooth Stack ID is Invalid during the StartScan() call

(-4) FUNCTION_ERROR

(-8) INVALID_STACK_ID_ERROR

(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID

(-1) BTPS_ERROR_INVALID_PARAMETER

(-56) BTPS_ERROR_GAP_NOT_INITIALIZED

(-104) BTPS_ERROR_LOCAL_CONTROLLER_DOES_NOT_SUPPORT_LE

(-57) BTPS_ERROR_DEVICE_HCI_ERROR

API Call

GAP_LE_Cancel_Scan(BluetoothStackID);

API Prototype

int BTPSAPI GAP_LE_Cancel_Scan(unsigned int BluetoothStackID);

Description of API

The GAP_LE_Cancel_Scan function is provided to allow the local host the ability to cancel (stop) an on-going scan procedure. This function will return zero if successful or a negative return error code if there was an error condition.


ConnectLE

Description

The ConnectLE command is responsible for connecting to an LE device. This command returns zero if successful and a negative value if an error occurred. This command calls the ConnectLEDevice(unsigned int BluetoothStackID, BD_ADDR_t BD_ADDR, Boolean_t UseWhiteList) function using ConnectLEDevice(BluetoothStackID, BD_ADDR, FALSE).

Parameters

The only parameter required is the Bluetooth Address of the remote device. This can easily be found using the StartScanning command if the advertising device is in proximity during the scan.

Command Call Examples

“ConnectLE 001bdc05b617” Attempts to send a connection request to the Bluetooth Device with the BD_ADDR of 001bdc05b617.

“ConnectLE 000275e126FF” Attempts to send a connection request to the Bluetooth Device with the BD_ADDR of 000275e126FF.

Possible Return Values

(0) Successfully Set Pairability Mode

(-4) FUNCTION_ERROR

(-6) INVALID_PARAMETERS_ERROR

(-8) INVALID_STACK_ID_ERROR

(-116) BTPS_ERROR_RANDOM_ADDRESS_IN_USE

(-111) BTPS_ERROR_CREATE_CONNECTION_OUTSTANDING

(-66) BTPS_ERROR_INSUFFICIENT_RESOURCES

(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID

(-1) BTPS_ERROR_INVALID_PARAMETER

(-56) BTPS_ERROR_GAP_NOT_INITIALIZED

(-104) BTPS_ERROR_LOCAL_CONTROLLER_DOES_NOT_SUPPORT_LE

(-57) BTPS_ERROR_DEVICE_HCI_ERROR

GAP_LE_ERROR_WHITE_LIST_IN_USE

API Calls

GAP_LE_Create_Connection(BluetoothStackID, 100, 100, Result?fpNoFilter:fpWhiteList, latPublic, Result?&BD_ADDR:NULL, latPublic, &ConnectionParameters, GAP_LE_Event_Callback, 0);

(these two APIs can generally be ignored unless the WhiteList is enabled in the call to ConnectLEDevice)

GAP_LE_Remove_Device_From_White_List(BluetoothStackID, 1, &WhiteListEntry, &WhiteListChanged);

GAP_LE_Add_Device_To_White_List(BluetoothStackID, 1, &WhiteListEntry, &WhiteListChanged);

API Prototypes

int BTPSAPI GAP_LE_Create_Connection(unsigned int BluetoothStackID, unsigned int ScanInterval, unsigned int ScanWindow, GAP_LE_Filter_Policy_t InitatorFilterPolicy, GAP_LE_Address_Type_t RemoteAddressType, BD_ADDR_t *RemoteDevice, GAP_LE_Address_Type_t LocalAddressType, GAP_LE_Connection_Parameters_t *ConnectionParameters, GAP_LE_Event_Callback_t GAP_LE_Event_Callback, unsigned long CallbackParameter);

int BTPSAPI GAP_LE_Remove_Device_From_White_List( unsigned int BluetoothStackID, unsigned int DeviceCount, GAP_LE_White_List_Entry_t *WhiteListEntries, unsigned int *RemovedDeviceCount);

int BTPSAPI GAP_LE_Add_Device_To_White_List(unsigned int BluetoothStackID, unsigned int DeviceCount, GAP_LE_White_List_Entry_t *WhiteListEntries, unsigned int *AddedDeviceCount);

Description of API

The GAP_LE_Create_Connection function is provided to allow the local host the ability to create a connection to a remote device using the Bluetooth LE radio. The connection process is asynchronous in nature and the caller will be notified via the GAP LE event callback function (specified in this function) when the connection completes. This function will return zero if successful, or a negative return error code if there was an error condition. The GAP_LE_Remove_Device_From_White_List function is provided to allow the local host the ability to remove one (or more) devices from the white list maintained by the local device. This function will attempt to delete as many devices as possible (from the specified list) and will return the number of devices deleted. The GAP_LE_Read_White_List_Size function can be used to determine how many devices the local device supports in the white list (simultaneously).


DisconnectLE

Description

The DisconnectLE command is responsible for disconnecting from an LE device. This command returns zero on successful execution and a negative value on all errors. This command requires that a valid Bluetooth Stack ID exists before running.

Parameters

The only parameter required is the Bluetooth Address of the remote device that is connected.

Command Call Examples

“DisconnectLE 001bdc05b617” Attempts to send a disconnection request to the Bluetooth Device with the BD_ADDR of 001bdc05b617.

“DisconnectLE 000275e126FF” Attempts to send a disconnection request to the Bluetooth Device with the BD_ADDR of 000275e126FF.

Possible Return Values

(0) Successfully disconnected remote device (-4) FUNCTION_ERROR (-8) INVALID_STACK_ID_ERROR

API Call

GAP_LE_Disconnect(BluetoothStackID, BD_ADDR);

API Prototype

int BTPSAPI GAP_LE_Disconnect(unsigned int BluetoothStackID, BD_ADDR_t BD_ADDR);

API Description

The GAP_LE_Disconnect function provides the ability to disconnect from a remote device. This function will return zero if successful, or a negative return error code if there was an error condition.


PairLE

Description

The PairLE command is provided to allow a mechanism of Pairing (or requesting security if a slave) to the connected device. This command calls the SendPairingRequest(BD_ADDR_t BD_ADDR, Boolean_t ConnectionMaster) function using SendPairingRequest(ConnectionBD_ADDR, LocalDeviceIsMaster).

Parameters

It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome of Pairing.

Possible Return Values

(0) Successfully Set Pairability Mode

(-4) FUNCTION_ERROR

(-6) INVALID_PARAMETERS_ERROR

(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID

(-1) BTPS_ERROR_INVALID_PARAMETER

(-56) BTPS_ERROR_GAP_NOT_INITIALIZED

(-104) BTPS_ERROR_LOCAL_CONTROLLER_DOES_NOT_SUPPORT_LE

(-66) BTPS_ERROR_INSUFFICIENT_RESOURCES

(-107) BTPS_ERROR_INVALID_DEVICE_ROLE_MODE

API Calls

GAP_LE_Pair_Remote_Device(BluetoothStackID, BD_ADDR, &Capabilities, GAP_LE_Event_Callback, 0);

GAP_LE_Request_Security(BluetoothStackID, BD_ADDR, Capabilities.Bonding_Type, Capabilities.MITM, GAP_LE_Event_Callback, 0);

API Prototypes

int BTPSAPI GAP_LE_Pair_Remote_Device(unsigned int BluetoothStackID, BD_ADDR_t BD_ADDR, GAP_LE_Pairing_Capabilities_t *Capabilities, GAP_LE_Event_Callback_t GAP_LE_Event_Callback, unsigned long CallbackParameter);

int BTPSAPI GAP_LE_Request_Security(unsigned int BluetoothStackID, BD_ADDR_t BD_ADDR, GAP_LE_Bonding_Type_t Bonding_Type, Boolean_t MITM, GAP_LE_Event_Callback_t GAP_LE_Event_Callback, unsigned long CallbackParameter);

Description of API

The GAP_LE_Pair_Remote_Device function is provided to allow a means to pair with a remote, connected, device. This function accepts the device address of the currently connected device to pair with, followed by the pairing capabilities of the local device. This function also accepts as input the GAP LE event callback information to use during the pairing process. This function returns zero if successful or a negative error code if there was an error. This function can only be issued by the master of the connection (the initiator of the connection). The reason is that a slave can only request a security procedure, it cannot initiate a security procedure. The GAP_LE_Request_Security function is provided to allow a means for a slave device to request that the master (of the connection) perform a pairing operation or re-establishing prior security. This function can only be called by a slave device. The reason for this is that the slave can only request for security to be initiated, it cannot initiate the security process itself. This function returns zero if successful or a negative error code if there was an error.


LEPassKeyResponse

Description

The LEPassKeyResponse command is responsible for issuing a GAP Authentication Response with a Pass Key value specified via the input parameter. This command returns zero on successful execution and a negative value on all errors.

Parameters

The PassKeyResponse command requires one parameter which is the Pass Key used for authenticating the connection. This is a string value which can be up to 6 digits long (with a value between 0 and 999999).

Command Call Examples

"PassKeyResponse 1234" Attempts to set the Pass Key to "1234.” "PassKeyResponse 999999" Attempts to set the Pass Key to "999999." This value represents the longest Pass Key value of 6 digits.

Possible Return Values

(0) Successful Pass Key Response

(-4) FUNCTION_ERROR

(-6) INVALID_PARAMETERS_ERROR

(-8) INVALID_STACK_ID_ERROR

(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID

(-1) BTPS_ERROR_INVALID_PARAMETER

(-118) BTPS_ERROR_PAIRING_NOT_ACTIVE

(-57) BTPS_ERROR_DEVICE_HCI_ERROR

(-56) BTPS_ERROR_GAP_NOT_INITIALIZED

(-104) BTPS_ERROR_LOCAL_CONTROLLER_DOES_NOT_SUPPORT_LE

(-66) BTPS_ERROR_INSUFFICIENT_RESOURCES

(-107) BTPS_ERROR_INVALID_DEVICE_ROLE_MODE

API Call

GAP_LE_Authentication_Response(BluetoothStackID, CurrentRemoteBD_ADDR, &GAP_LE_Authentication_Response_Information);

API Prototype

int BTPSAPI GAP_LE_Authentication_Response(unsigned int BluetoothStackID, BD_ADDR_t BD_ADDR, GAP_LE_Authentication_Response_Information_t *GAP_LE_Authentication_Information);

Description of API

This function is provided to allow a mechanism for the local device to respond to GAP LE authentication events. This function is used to specify the authentication information for the specified Bluetooth device. This function accepts as input, the Bluetooth protocol stack ID of the Bluetooth device that has requested the authentication action, and the authentication response information (specified by the caller).


LEQueryEncryption

Description

The LEQueryEncryption command is responsible for quering the Encryption Mode for an LE Connection. This command returns zero on successful execution and a negative value on all errors.

Parameters

It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome of the Query.

Possible Return Values

(0) Successfully Queried Encryption Mode

(-4) FUNCTION_ERROR

(-8) INVALID_STACK_ID_ERROR

(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID

(-1) BTPS_ERROR_INVALID_PARAMETER

(-56) BTPS_ERROR_GAP_NOT_INITIALIZED

(-104) BTPS_ERROR_LOCAL_CONTROLLER_DOES_NOT_SUPPORT_LE

API Call

GAP_LE_Query_Encryption_Mode(BluetoothStackID, ConnectionBD_ADDR, &GAP_Encryption_Mode);

API Prototype

int BTPSAPI GAP_LE_Query_Encryption_Mode(unsigned int BluetoothStackID, BD_ADDR_t BD_ADDR, GAP_Encryption_Mode_t *GAP_Encryption_Mode);

Description of API

This function is provided to allow a means to query the current encryption mode for the LE connection that is specified.


SetPasskey

Description

The SetPasskey command is responsible for querying the Encryption Mode for an LE Connection. This command returns zero on successful execution and a negative value on all errors.

Note: SetPasskey Command works only when you are pairing.

Parameters

The SetPasskey command requires one parameter which is the Pass Key used for authenticating the connection. This is a string value which can be up to 6 digits long (with a value between 0 and 999999).

Command Call Examples

“SetPasskey 0” Attempts to remove the Passkey.

“SetPasskey 1 987654” Attempts to set the Passkey to 987654.

“SetPasskey 1” Attempts to set the Passkey to the default Fixed Passkey value.

Possible Return Values

(0) Successful Pass Key Response

(-4) FUNCTION_ERROR

(-6) INVALID_PARAMETERS_ERROR

(-8) INVALID_STACK_ID_ERROR

(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID

(-1) BTPS_ERROR_INVALID_PARAMETER

(-56) BTPS_ERROR_GAP_NOT_INITIALIZED

(-104) BTPS_ERROR_LOCAL_CONTROLLER_DOES_NOT_SUPPORT_LE

API Calls

(Depending on the First Parameter one of these will be chosen)

GAP_LE_Set_Fixed_Passkey(BluetoothStackID, &Passkey);

GAP_LE_Set_Fixed_Passkey(BluetoothStackID, NULL);

API Prototype

int BTPSAPI GAP_LE_Set_Fixed_Passkey(unsigned int BluetoothStackID, DWord_t *Fixed_Display_Passkey);

Description of API

This function is provided to allow a means for a fixed passkey to be used whenever the local Bluetooth device is chosen to display a passkey during a pairing operation. This fixed passkey is only used when the local Bluetooth device is chosen to display the passkey, based on the remote I/O Capabilities and the local I/O capabilities.


DiscoverGAPS

Description

The DiscoverGAPS command is provided to allow an easy mechanism to start a service discovery procedure to discover the Generic Access Profile Service on the connected remote device.

Parameters

It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome of the service discovery.

Possible Return Values

(0) Successfully discovered the Generic Access Profile Service.

(-4) Function Error (on failure).

API Call

GDIS_Service_Discovery_Start(BluetoothStackID, ConnectionID, (sizeof(UUID)/sizeof(GATT_UUID_t)), UUID, GDIS_Event_Callback, sdGAPS)

API Prototypes

int BTPSAPI GDIS_Service_Discovery_Start(unsigned int BluetoothStackID, unsigned int ConnectionID, unsigned int NumberOfUUID, GATT_UUID_t *UUIDList, GDIS_Event_Callback_t ServiceDiscoveryCallback, unsigned long ServiceDiscoveryCallbackParameter)

Description of API

The GDIS_Service_Discover_Start is in an application module called GDIS that is provided to allow an easy way to perform GATT service discovery. This module can and should be modified for the customers use. This function is called to start a service discovery operation by the GDIS module.


GetLocalName

Description

The GetLocalName command is responsible for querying the name of the local Bluetooth Device. This command returns zero on a successful execution and a negative value on all errors. A Bluetooth Stack ID must exist before attempting to call this command.

Parameters

It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome of the Query.

Possible Return Values

(0) Successfully Queried Local Device Name

(-8) INVALID_STACK_ID_ERROR

(-4) FUNCTION_ERROR

(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID

(-1) BTPS_ERROR_INVALID_PARAMETER

(-57) BTPS_ERROR_DEVICE_HCI_ERROR

(-65) BTPS_ERROR_INSUFFICIENT_BUFFER_SPACE

API Call

GAP_Query_Local_Device_Name(BluetoothStackID, 257, (char *)LocalName);

API Prototype

int BTPSAPI GAP_Query_Local_Device_Name(unsigned int BluetoothStackID, unsigned int NameBufferLength, char *NameBuffer);

Description of API

This function is responsible for querying (and reporting) the user friendly name of the local Bluetooth device. The final parameters to this function specify the buffer and buffer length of the buffer that is to receive the local device name. The NameBufferLength parameter should be at least (MAX_NAME_LENGTH+1) to hold the maximum allowable device name (plus a single character to hold the NULL terminator). If this function is successful, this function returns zero, and the buffer that NameBuffer points to will be filled with a NULL terminated ASCII representation of the local device name. If this function returns a negative value, then the local device name was NOT able to be queried (error condition).


SetLocalName

Description

The SetLocalName command is responsible for setting the name of the local Bluetooth Device to a specified name. This command returns zero on a successful execution and a negative value on all errors. A Bluetooth Stack ID must exist before attempting to call this command.

Parameters

One parameter is necessary for this command. The specified device name must be the only parameter (which means there should not be spaces in the name or only the first section of the name will be set).

Command Call Examples

"SetLocalName New_Bluetooth_Device_Name" Attempts to set the Local Device Name to "New_Bluetooth_Device_Name." "SetLocalName New Bluetooth Device Name" Attempts to set the Local Device Name to "New Bluetooth Device Name" but only sets the first parameter, which would make the Local Device Name "New." "SetLocalName MSP430" Attempts to set the Local Device Name to "MSP430."

Possible Return Values

(0) Successfully Set Local Device Name

(-1) BTPS_ERROR_INVALID_PARAMETER

(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID

(-8) INVALID_STACK_ID_ERROR

(-4) FUNCTION_ERROR

(-57) BTPS_ERROR_DEVICE_HCI_ERROR

API Call

GAP_Set_Local_Device_Name(BluetoothStackID, TempParam->Params[0].strParam);

API Prototype

int BTPSAPI GAP_Set_Local_Device_Name(unsigned int BluetoothStackID, char *Name);

Description of API

This function is provided to allow the changing of the device name of the local Bluetooth device. The Name parameter must be a pointer to a NULL terminated ASCII string of at most MAX_NAME_LENGTH (not counting the trailing NULL terminator). This function will return zero if the local device name was successfully changed, or a negative return error code if there was an error condition.


GetRemoteName

Description

The GetRemoteName command is responsible for querying the Bluetooth Device Name of a Remote Device. This command returns zero on a successful execution and a negative value on all errors. The command requires that a valid Bluetooth Stack ID exists before running and it should be called after using the Inquiry command. The DisplayInquiryList command would be useful in this situation to find which Remote Device goes with which Inquiry Index.

Parameters

The GetRemoteName command requires one parameter which is the Inquiry Index of the Remote Bluetooth Device. This value can be found after an Inquiry or displayed when the command DisplayInquiryList is used. Command Call Examples "GetRemoteName 5" Attempts to query the Device Name for the Remote Device that is at the fifth Inquiry Index. "GetRemoteName 8" Attempts to query the Device Name for the Remote Device that is at the eighth Inquiry Index.

Possible Return Values

(0) Successfully Queried Remote Name

(-6) INVALID_PARAMETERS_ERROR

(-4) FUNCTION_ERROR

(-8) INVALID_STACK_ID_ERROR

(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID

(-1) BTPS_ERROR_INVALID_PARAMETER

(-59) BTPS_ERROR_ADDING_CALLBACK_INFORMATION

(-57) BTPS_ERROR_DEVICE_HCI_ERROR

API Call

GAP_Query_Remote_Device_Name(BluetoothStackID, InquiryResultList[(TempParam->Params[0].intParam – 1)], GAP_Event_Callback, (unsigned long)0);

API Prototype

int BTPSAPI GAP_Query_Remote_Device_Name(unsigned int BluetoothStackID, BD_ADDR_t BD_ADDR, GAP_Event_Callback_t GAP_Event_Callback, unsigned long CallbackParameter);

Description of API

This function is provided to allow a mechanism to query the user-friendly Bluetooth device name of the specified remote Bluetooth device. This function accepts as input the Bluetooth device address of the remote Bluetooth device to query the name of and the GAP event callback information that is to be used when the remote device name process has completed. This function returns zero if successful, or a negative return error code if the remote name request was unable to be submitted. If this function returns success, then the caller will be notified via the specified callback when the remote name information has been determined (or there was an error). This function cannot be used to determine the user-friendly name of the local Bluetooth device. The GAP_Query_Local_Name function should be used to query the user-friendly name of the local Bluetooth device. Because this function is asynchronous in nature (specifying a remote device address), this function will notify the caller of the result via the specified callback. The caller is free to cancel the remote name request at any time by issuing the GAP_Cancel_Query_Remote_Name function and specifying the Bluetooth device address of the Bluetooth device that was specified in the original call to this function. It should be noted that when the callback is cancelled, the operation is attempted to be cancelled and the callback is cancelled (i.e. the GAP module still might perform the remote name request, but no callback is ever issued).


LEUserConfirmationResponse

Description

The LEUserConfirmationResponse command is responsible for issuing a GAP LE Authentication Response with a User Confirmation value specified via the input parameter. This function returns zero on successful execution and a negative value on all errors.

Parameters

This command requires one parameter which indicates if confirmation is accepted or not. 0 = decline, 1 = accept.

Command Call Examples

“LEUserConfirmationResponse 0” Attempts to Response with a decline value.

“LEUserConfirmationResponse 1” Attempts to Response with a accept value.

Possible Return Values

(0) Success.

(-4) FUNCTION_ERROR.

(-6) INVALID_PARAMETERS_ERROR.

(-1) BTPS_ERROR_INVALID_PARAMETER.

(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID.

(-56) BTPS_ERROR_GAP_NOT_INITIALIZED.

(-57) BTPS_ERROR_DEVICE_HCI_ERROR.

(-66) BTPS_ERROR_INSUFFICIENT_RESOURCES.

(-98) BTPS_ERROR_DEVICE_NOT_CONNECTED.

(-103) BTPS_ERROR_FEATURE_NOT_AVAILABLE.

(-104) BTPS_ERROR_LOCAL_CONTROLLER_DOES_NOT_SUPPORT_LE.

(-107) BTPS_ERROR_INVALID_DEVICE_ROLE_MODE.

(-118) BTPS_ERROR_PAIRING_NOT_ACTIVE.

(-119) BTPS_ERROR_INVALID_STATE.

(-120) BTPS_ERROR_FEATURE_NOT_CURRENTLY_ACTIVE.

(-122) BTPS_ERROR_NUMERIC_COMPARISON_FAILED.

API Call

GAP_LE_Authentication_Response(BluetoothStackID, CurrentLERemoteBD_ADDR, &GAP_LE_Authentication_Response_Information)

API Prototype

int BTPSAPI GAP_LE_Authentication_Response(unsigned int BluetoothStackID, BD_ADDR_t BD_ADDR, GAP_LE_Authentication_Response_Information_t *GAP_LE_Authentication_Information)

Description of API

The following function is provided to allow a mechanism for the local device to respond to GAP LE authentication events. This function is used to set the authentication information for the specified Bluetooth device. This function accepts as input, the Bluetooth protocol stack ID followed by the remote Bluetooth device address that is currently executing a pairing/authentication process, followed by the authentication response information.This function returns zero if successful, or a negative return error code if there was an error.


EnableSCOnly

Description

The EnableSCOnly command enables LE Secure Connections (SC) only mode. In case this mode is enabled, pairing request from peers that support legacy pairing only will be rejected. Please note that in case this mode is enabled, the SC flag in the LE_Parameters must be set to TRUE. This function returns zero on successful execution and a negative value on all errors.

Parameters

This command requires one parameter which indicates if Secure connections only mode is set or not. 0 = SC Only mode is off, 1 = SC Only mode is on.

Command Call Examples

“EnableSCOnly 0” Disable Secure connections only mode.

“EnableSCOnly 1” Enable Secure connections only mode.

Possible Return Values

(0) Success.

(-4) FUNCTION_ERROR.

(-6) INVALID_PARAMETERS_ERROR.

(-8) INVALID_STACK_ID_ERROR.

(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID.

(-56) BTPS_ERROR_GAP_NOT_INITIALIZED.

(-103) BTPS_ERROR_FEATURE_NOT_AVAILABLE.

(-104) BTPS_ERROR_LOCAL_CONTROLLER_DOES_NOT_SUPPORT_LE.

(-120) BTPS_ERROR_FEATURE_NOT_CURRENTLY_ACTIVE.

API Call

GAP_LE_SC_Only_Mode(BluetoothStackID, EnableSCOnly)

API Prototype

int BTPSAPI GAP_LE_SC_Only_Mode(unsigned int BluetoothStackID, Boolean_t EnableSCOnly)

Description of API

The following function is provided to allow a configuration of LE Secure Connecions only mode. The upper layer will use this function before the beginning of LE SC pairing, in case it asks to reject a device that supports only legacy pairing. This mode should be used when it is more important for a device to have high security than it is for it to maintain backwards compatibility with devices that do not support SC. This function accepts as parameters the Bluetooth stack ID of the Bluetooth device,and a boolean EnableSCOnly that enable or disable the SC only mode. This function should be used ones, before the first pairing process. This function returns zero if successful or a negative error code.


RegenerateP256LocalKeys

Description

The following function allows the user to generate new P256 private and local keys. This function shall NOT be used in the middle of a pairing process. It is relevant for LE Secure Conenctions pairing only! This function returns zero on successful execution and a negative value on all errors.

Parameters

No parameters are necessary.

Command Call Examples

“RegenerateP256LocalKeys” Attempts to generate new P256 private and local keys.

Possible Return Values

(0) Success.

(-4) FUNCTION_ERROR.

(-8) INVALID_STACK_ID_ERROR.

(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID.

(-56) BTPS_ERROR_GAP_NOT_INITIALIZED.

(-104) BTPS_ERROR_LOCAL_CONTROLLER_DOES_NOT_SUPPORT_LE.

(-117) BTPS_ERROR_PAIRING_ACTIVE.

(-120) BTPS_ERROR_FEATURE_NOT_CURRENTLY_ACTIVE.

API Call

GAP_LE_SC_Regenerate_P256_Local_Keys(BluetoothStackID)

API Prototype

int BTPSAPI GAP_LE_SC_Regenerate_P256_Local_Keys(unsigned int BluetoothStackID)

Description of API

The following function is provided to allow a regeneration of the P-256 private and local puclic keys. This function is relevant only in case of LE SC pairing. This function accepts as parameters the Bluetooth stack ID of the Bluetooth device. This functions shall NOT be used while performing pairing. This function returns zero if successful or a negative error code.


SCGenerateOOBLocalParams

Description

In order to be able to perform LE SC pairing in OOB method we need to generate local random and confirmation values before the pairing process starts. The following function allows the user to generate OOB local parameters. This function shall NOT be used in the middle of a pairing process. It is relevant for LE SC pairing only! This function returns zero on successful execution and a negative value on all errors.

Parameters

No parameters are necessary.

Command Call Examples

“SCGenerateOOBLocalParams” Attempts to generate local random and confirmation values before the pairing process starts.

Possible Return Values

(0) Success.

(-4) FUNCTION_ERROR.

(-8) INVALID_STACK_ID_ERROR.

(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID.

(-56) BTPS_ERROR_GAP_NOT_INITIALIZED.

(-104) BTPS_ERROR_LOCAL_CONTROLLER_DOES_NOT_SUPPORT_LE.

(-117) BTPS_ERROR_PAIRING_ACTIVE.

(-120) BTPS_ERROR_FEATURE_NOT_CURRENTLY_ACTIVE.

API Call

GAP_LE_SC_OOB_Generate_Parameters(BluetoothStackID, &OOBLocalRandom, &OOBLocalConfirmation)

API Prototype

int BTPSAPI GAP_LE_SC_OOB_Generate_Parameters(unsigned int BluetoothStackID, SM_Random_Value_t *OOB_Local_Rand_Result, SM_Confirm_Value_t *OOB_Local_Confirm_Result)

Description of API

The following function is provided to allow the use of LE Secure Connections (SC) pairing in Out Of Band (OOB) association method. The upper layer will use this function to generate the the local OOB random value, and OOB confirmation value (ra/rb and Ca/Cb) as defined in the Bluetooth specification. This function accepts as parameters the Bluetooth stack ID of the Bluetooth device, and pointers to buffers that will recieve the generated local OOB random, and OOB confirmation values. This function returns zero if successful or a negative error code.


SetLocalAppearence

Description

The SetLocalAppearence command is provided to set the local device appearance that is exposed by the GAP Service (GAPS).

Parameters

The SetLocalAppearence command requires one parameter which is the Local Device Appearance you wish to be set.

Possible Return Values

(0) Success.

(-4) Function error (on failure).

API Call

GAPS_Set_Device_Appearance(BluetoothStackID, GAPSInstanceID, Appearance)

API Prototype

int BTPSAPI GAPS_Set_Device_Appearance(unsigned int BluetoothStackID, unsigned int InstanceID, Word_t DeviceAppearance);

Description of API

This function allows a mechanism of setting the local device appearance that is exposed as part of the GAP Service API (GAPS).


GetLocalAppearence

Description

The GetLocalAppearence command is provided to read the local device appearance that is exposed by the GAP Service (GAPS).

Parameters

It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome.

Possible Return Values

(0) Success.

(-4) Function error (on failure).

API Call

GAPS_Query_Device_Appearance(BluetoothStackID, GAPSInstanceID, &Appearance)

API Prototype

int BTPSAPI GAPS_Query_Device_Appearance(unsigned int BluetoothStackID, unsigned int InstanceID, Word_t *DeviceAppearance)

Description of API

This function allows a mechanism of reading the local device appearance that is exposed as part of the GAP Service API (GAPS).


GetRemoteAppearence

Description

The GetRemoteAppearence command is provided to read the device appearance from the connected remote device that is exposed as part of the GAP Service. The GAP Service on the remote device must have already been discovered using the DiscoverGAPS command.

Parameters

It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome

Possible Return Values

(0) Success.

(-4) Function error (on failure).

API Call

GATT_Read_Value_Request(BluetoothStackID, ConnectionID, DeviceInfo->GAPSClientInfo.DeviceAppearanceHandle, GATT_ClientEventCallback_GAPS, (unsigned long)DeviceInfo->GAPSClientInfo.DeviceAppearanceHandle)

API Prototype

int BTPSAPI GATT_Read_Value_Request(unsigned int BluetoothStackID, unsigned int ConnectionID, Word_t AttributeHandle, GATT_Client_Event_Callback_t ClientEventCallback, unsigned long CallbackParameter)

Description of API

This function allows a mechanism of reading an attribute from a connected device.


SPPLE Commands
DiscoverSPPLE

Description

The following function is responsible for performing a SPPLE Service Discovery Operation. This function will return zero on successful execution and a negative value on errors.

Parameters

The only parameter required is the Bluetooth Address of the remote device that is connected.

Command Call Examples

“DiscoverSPPLE 001bdc05b617” Attempts to discover services of the Bluetooth Device with the BD_ADDR of 001bdc05b617.

“DiscoverSPPLE 000275e126FF” Attempts to discover services of the Bluetooth Device with the BD_ADDR of 000275e126FF.

Possible Return Values

(0) Successfully started a SPP LE Service Discovery.

(-4) Function Error (on failure).

API Call

GDIS_Service_Discovery_Start(BluetoothStackID, ConnectionID, (sizeof(UUID)/sizeof(GATT_UUID_t)), UUID, GDIS_Event_Callback, 0)

API Prototype

int BTPSAPI GDIS_Service_Discovery_Start(unsigned int BluetoothStackID, unsigned int ConnectionID, unsigned int NumberOfUUID, GATT_UUID_t *UUIDList, GDIS_Event_Callback_t ServiceDiscoveryCallback, unsigned long ServiceDiscoveryCallbackParameter)

Description of API

The GDIS_Service_Discover_Start is in an application module called GDIS that is provided to allow an easy way to perform GATT service discovery. This function is called to start a service discovery operation by the GDIS module.


RegisterSPPLE

Description

The following function is responsible for registering a SPPLE Service. This function will return zero on successful execution and a negative value on errors.

Parameters

It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome of registering a SPPLE Service.

Possible Return Values

(0) Successfully registered a SPPLE Service.

(-4) Function Error (on failure).

API Call

GATT_Register_Service(BluetoothStackID, SPPLE_SERVICE_FLAGS, SPPLE_SERVICE_ATTRIBUTE_COUNT, (GATT_Service_Attribute_Entry_t *)SPPLE_Service, &ServiceHandleGroup, GATT_ServerEventCallback, 0)

API Prototype

int BTPSAPI GATT_Register_Service(unsigned int BluetoothStackID, Byte_t ServiceFlags, unsigned int NumberOfServiceAttributeEntries, GATT_Service_Attribute_Entry_t *ServiceTable, GATT_Attribute_Handle_Group_t *ServiceHandleGroupResult, GATT_Server_Event_Callback_t ServerEventCallback, unsigned long CallbackParameter)

Description of API

The following function is provided to allow a means to add a GATT Service to the local GATT Database. The first parameter is Bluetooth stack ID of the Bluetooth Device. The second parameter is a bit mask field that specifies the type of service being registered, which must be non-zero (i.e. at least one bit must be set). The third parameter is the number of entries in the service attribute array that is pointed to by the fourth parameter. The fourth parameter is an array that contains the attributes for the service being registered. The next parameter is a pointer to a buffer that will store the attribute handle range of the registered service. The final two parameters specify the GATT server callback and callback parameter that will be used whenever a client request to the GATT server cannot be satisified internally by the local GATT module. This function will return a positive non-zero service ID if successful, or a negative return error code if there was an error. If this function returns success then the ServiceHandleGroupResult buffer will contain the service's attribute handle range.


LESend

Description

The following function is responsible for sending a number of characters to a remote device to which a connection exists. The function receives a parameter that indicates the number of byte to be transferred. This function will return zero on successful execution and a negative value on errors. Depending what the device role for SPPLE is, server or client, the API function that is called is either a GATT_Handle_Value_Notification or a GATT_Write_Without_Response_Request; which notifies the receiving credit characteristic or sends a write with out response packet to the transmission credit characteristic respectively.

Parameters

Lesend requires two parameters. The first is the remote Bluetooth address of the device you are sending to. The second is the number of bytes to send. This value has to be greater than 10.

Command Call Examples

"LeSend 0017E7FEFD7C 100" Attempts to send 100 bytes of data to 0017E7FEFD7C.

"LeSend B8FFFEAF1CAD 25" Attempts to send 25 bytes of data to B8FFFEAF1CAD.

Possible Return Values

(0) Successfully Sent Data

(-1) BTPS_ERROR_INVALID_PARAMETER

(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID

(-67) BTPS_ERROR_RFCOMM_NOT_INITIALIZED

(-85) BTPS_ERROR_SPP_NOT_INITIALIZED

API Call

GATT_Handle_Value_Notification(BluetoothStackID, SPPLEServiceID, ConnectionID, SPPLE_TX_CHARACTERISTIC_ATTRIBUTE_OFFSET, (Word_t)DataCount, SPPLEBuffer)

OR

GATT_Write_Without_Response_Request(BluetoothStackID, ConnectionID, DeviceInfo->ClientInfo.Rx_Characteristic, (Word_t)DataCount, SPPLEBuffer)

API Prototype

int BTPSAPI GATT_Handle_Value_Notification(unsigned int BluetoothStackID, unsigned int ServiceID, unsigned int ConnectionID, Word_t AttributeOffset, Word_t AttributeValueLength, Byte_t *AttributeValue)

OR

int BTPSAPI GATT_Write_Without_Response_Request(unsigned int BluetoothStackID, unsigned int ConnectionID, Word_t AttributeHandle, Word_t AttributeLength, void *AttributeValue)

Description of API

The first of these API functions allows a means of sending a Handle/Value notification to a remote GATT client. The first parameter to this function is the Bluetooth stack ID of the local Bluetooth stack. The second parameter is the service ID of the service that is sending the Handle/Value notification. The third parameter specifies the connection ID of the connection to send the Handle/Value notification to. The fourth parameter specifies the offset in the service table (registered via the call to the GATT_Register_Service() function) of the attribute that is being notified. The fifth parameter is the length (in bytes) of the attribute value that is being notified. The sixth parameter is a pointer to the actual attribute value to notify. This function will return a non-negative value that represents the actual length of the attribute value that was notified, or a negative return error code if there was an error.

The second of these API functions is provided to allow a means of performing a write without response request to remote device for a specified attribute. The first parameter to this function is the Bluetooth stack ID of the local Bluetooth stack, followed by the connection ID of the connected remote device, followed by the handle of the attribute to write, followed by the length of the value data to write (in bytes), followed by the actual value to write. This function will return the number of bytes written on success or a negative error code.

ConfigureSPPLE

Description

The following function is responsible to configure a SPPLE Service on a remote device. This function will return zero on successful execution and a negative value on errors. The following function enables notifications of the proper characteristics based on a specified handle; depending what the device role for SPPLE is, server or client, the API function that is called is either a GATT_Handle_Value_Notification or a GATT_Write_Without_Response_Request; which notifies the receiving credit characteristic or sends a write with out response packet to the transmission credit characteristic respectively.

Parameters

The only parameter required is the Bluetooth Address of the remote device that is connected.

Command Call Examples

“ConfigureSPPLE 001bdc05b617” Attempts to configure services of the Bluetooth Device with the BD_ADDR of 001bdc05b617.

“ConfigureSPPLE 000275e126FF” Attempts to configure services of the Bluetooth Device with the BD_ADDR of 000275e126FF.

Possible Return Values

(0) Successfully configured a SPPLE Service.

(-4) Function Error (on failure).

API Call

GATT_Write_Request(BluetoothStackID, ConnectionID, ClientConfigurationHandle, sizeof(Buffer), &Buffer, ClientEventCallback, 0)

AND

GATT_Handle_Value_Notification(BluetoothStackID, SPPLEServiceID, ConnectionID, SPPLE_RX_CREDITS_CHARACTERISTIC_ATTRIBUTE_OFFSET, WORD_SIZE, (Byte_t *)&Credits)

OR

GATT_Write_Without_Response_Request(BluetoothStackID, ConnectionID, DeviceInfo->ClientInfo.Tx_Credit_Characteristic, WORD_SIZE, &Credits)

API Prototype

int BTPSAPI GATT_Write_Request(unsigned int BluetoothStackID, unsigned int ConnectionID, Word_t AttributeHandle, Word_t AttributeLength, void *AttributeValue, GATT_Client_Event_Callback_t ClientEventCallback, unsigned long CallbackParameter)

AND

int BTPSAPI GATT_Handle_Value_Notification(unsigned int BluetoothStackID, unsigned int ServiceID, unsigned int ConnectionID, Word_t AttributeOffset, Word_t AttributeValueLength, Byte_t *AttributeValue)

OR

int BTPSAPI GATT_Write_Without_Response_Request(unsigned int BluetoothStackID, unsigned int ConnectionID, Word_t AttributeHandle, Word_t AttributeLength, void *AttributeValue)

Description of API

The first of these API functions is provided to allow a means of performing a write request to a remote device for a specified attribute. The first parameter to this function is the Bluetooth stack ID of the local Bluetooth stack, followed by the connection ID of the connected remote device, followed by the handle of the attribute to write the value of, followed by the length of the value (in bytes), followed by the the actual value data to write. The final two parameters specify the GATT client event callback function and callback parameter (respectively) that will be called when a response is received from the remote device. This function will return the positive, non-zero, Transaction ID of the request or a negative error code.

The second of these API functions allows a means of sending a Handle/Value notification to a remote GATT client. The first parameter to this function is the Bluetooth stack ID of the local Bluetooth stack. The second parameter is the service ID of the service that is sending the Handle/Value notification. The third parameter specifies the connection ID of the connection to send the Handle/Value notification to. The fourth parameter specifies the offset in the service table (registered via the call to the GATT_Register_Service() function) of the attribute that is being notified. The fifth parameter is the length (in bytes) of the attribute value that is being notified. The sixth parameter is a pointer to the actual attribute value to notify. This function will return a non-negative value that represents the actual length of the attribute value that was notified, or a negative return error code if there was an error.

The third of these API functions is provided to allow a means of performing a write without response request to remote device for a specified attribute. The first parameter to this function is the Bluetooth stack ID of the local Bluetooth stack, followed by the connection ID of the connected remote device, followed by the handle of the attribute to write, followed by the length of the value data to write (in bytes), followed by the actual value to write. This function will return the number of bytes written on success or a negative error code.


LERead

Description

The following function is responsible for reading data sent by a remote device to which a connection exists. This function will return zero on successful execution and a negative value on errors. Depending what the device role for SPPLE is, server or client, the API function that is called is either a GATT_Handle_Value_Notification or a GATT_Write_Without_Response_Request; which notifies the receiving credit characteristic or sends a write with out response packet to the transmission credit characteristic respectively.

Parameters

The only parameter required is the Bluetooth Address of the remote device that is connected.

Command Call Examples

“LeRead 001bdc05b617” Attempts to read data of the Bluetooth Device with the BD_ADDR of 001bdc05b617.

“LeRead 000275e126FF” Attempts to read data of the Bluetooth Device with the BD_ADDR of 000275e126FF.

Possible Return Values

(0) Successfully Read Data

(-6) INVALID_PARAMETERS_ERROR

(-1) BTPS_ERROR_INVALID_PARAMETER

(-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID

(-67) BTPS_ERROR_RFCOMM_NOT_INITIALIZED

(-85) BTPS_ERROR_SPP_NOT_INITIALIZED

(-86) BTPS_ERROR_SPP_PORT_NOT_OPENED

API Call

GATT_Handle_Value_Notification(BluetoothStackID, SPPLEServiceID, ConnectionID, SPPLE_RX_CREDITS_CHARACTERISTIC_ATTRIBUTE_OFFSET, WORD_SIZE, (Byte_t *)&Credits)

OR

GATT_Write_Without_Response_Request(BluetoothStackID, ConnectionID, DeviceInfo->ClientInfo.Tx_Credit_Characteristic, WORD_SIZE, &Credits)

API Prototype

int BTPSAPI GATT_Handle_Value_Notification(unsigned int BluetoothStackID, unsigned int ServiceID, unsigned int ConnectionID, Word_t AttributeOffset, Word_t AttributeValueLength, Byte_t *AttributeValue)

OR

int BTPSAPI GATT_Write_Without_Response_Request(unsigned int BluetoothStackID, unsigned int ConnectionID, Word_t AttributeHandle, Word_t AttributeLength, void *AttributeValue)

Description of API

The first of these API functions allows a means of sending a Handle/Value notification to a remote GATT client. The first parameter to this function is the Bluetooth stack ID of the local Bluetooth stack. The second parameter is the service ID of the service that is sending the Handle/Value notification. The third parameter specifies the connection ID of the connection to send the Handle/Value notification to. The fourth parameter specifies the offset in the service table (registered via the call to the GATT_Register_Service() function) of the attribute that is being notified. The fifth parameter is the length (in bytes) of the attribute value that is being notified. The sixth parameter is a pointer to the actual attribute value to notify. This function will return a non-negative value that represents the actual length of the attribute value that was notified, or a negative return error code if there was an error.

The second of these API functions is provided to allow a means of performing a write without response request to remote device for a specified attribute. The first parameter to this function is the Bluetooth stack ID of the local Bluetooth stack, followed by the connection ID of the connected remote device, followed by the handle of the attribute to write, followed by the length of the value data to write (in bytes), followed by the actual value to write. This function will return the number of bytes written on success or a negative error code.


Loopback

Description

The Loopback command is responsible for setting the application state to support loopback mode. This command will return zero on successful execution and a negative value on errors.

Parameters

This command requires one parameter which indicates if loopback should be supported. 0 = loopback not active, 1 = loopback active.

Command Call Examples

"Loopback 0" sets loopback support to inactive.

"loopback 1" sets loopback support to active.

Possible Return Values

(0) Successfully set loopback support.

(-6) INVALID_PARAMETERS_ERROR


DisplayRawModeData

Description

The following function is responsible for setting the application state to support displaying Raw Data. This function will return zero on successful execution and a negative value on errors.

Parameters

This command accepts one parameter which indicates if displaying raw data mode should be supported. 0 = Display Raw Data Mode inactive, 1 = Display Raw Data active.

Command Call Examples

"DisplayRawModeData 0" sets Display Raw Mode support inactive.

"DisplayRawModeData 1" sets Display Raw Mode support active.

Possible Return Values

(0) Successfully sets Display Raw Data Mode support.

(-6) INVALID_PARAMETERS_ERROR


AutomaticReadMode

Description

The AutomaticReadMode command is responsible for setting the application state to support Automatically reading all data that is received through SPP. This function will return zero on successful execution and a negative value on errors.

Parameters

This command accepts one parameter which indicates if automatic read mode should be supported. 0 = Automatic Read Mode inactive, 1 = Automatic Read Mode active.

Command Call Examples

"AutomaticReadMode 0" sets Automatic Read Mode support to inactive.

"AutomaticReadMode 1" sets Automatic Read Mode support to active.

Possible Return Values

(0) Successfully set Automatic Read Mode support.

(-6) INVALID_PARAMETERS_ERROR