SWRU580 April   2021 CC2564C , CC2564MODA , CC2564MODN

 

  1.   Trademarks
  2. 1 Introduction
  3. 2 A2DP (AUD) Demo Guide
    1. 2.1 Demo Overview
    2. 2.2 Demo Application
    3. 2.3 Application Commands
  4. 3 A3DP Sink Demo Guide
    1. 3.1 Demo Overview
    2. 3.2 Demo Application
    3. 3.3 Sink Reference Board Demo Application
    4. 3.4 Multiple Source Demo
    5. 3.5 Application Commands
  5. 4 A3DP Source Demo Guide
    1. 4.1 Demo Overview
    2. 4.2 Demo Application
    3. 4.3 Application Commands
  6. 5 HFP Demo Guide
    1. 5.1 Demo Overview
    2. 5.2 Demo Application
    3. 5.3 Application Commands
  7. 6 HFP Audio Gateway Demo Guide
    1. 6.1 Demo Overview
    2. 6.2 Demo Application
    3. 6.3 Application Commands
  8. 7 HID Demo Guide
    1. 7.1 Demo Overview
    2. 7.2 Demo Application
    3. 7.3 Application Commands
  9. 8 HSP Demo Guide
    1. 8.1 Demo Overview
    2. 8.2 Demo Application
    3. 8.3 Application Command
  10. 9 Map Demo Guide
    1. 9.1 Demo Overview
    2. 9.2 Demo Application
    3. 9.3 Application Command
  11. 10PBAP Demo Guide
    1. 10.1 Demo Overview
    2. 10.2 Demo Application
    3. 10.3 Application Commands
  12. 11SPP Demo Guide
    1. 11.1 Demo Overview
    2. 11.2 Demo Application
    3. 11.3 Application Commands
  13. 12SPPLE Demo Guide
    1. 12.1 Demo Overview
    2. 12.2 Demo Application
    3. 12.3 Demonstrating SPP LE on an iOS Device with the LightBlue App
    4. 12.4 Demonstrating SPP LE on an iOS Device with the SPPLE Transfer App - LEGACY
    5. 12.5 SPP Demo
    6. 12.6 Application Commands
  14. 13SPPDMMulti Demo Guide
    1. 13.1 Demo Overview
    2. 13.2 Demo Application
    3. 13.3 Application Commands
  15. 14ANP Demo Guide
    1. 14.1 Demo Overview
    2. 14.2 Demo Application
    3. 14.3 Application Commands
  16. 15HFP Demo Guide
    1. 15.1 Demo Overview
    2. 15.2 Demo Application
    3. 15.3 Application Commands
  17. 16HTP Demo Guide
    1. 16.1 Demo Overview
    2. 16.2 Demo Application
    3. 16.3 Application Commands
  18. 17PASP Demo Guide
    1. 17.1 Demo Overview
    2. 17.2 Demo Application
    3. 17.3 Application Commands
  19. 18HOGP Demo Guide
    1. 18.1 Demo Overview
    2. 18.2 Demo Application
    3. 18.3 Application Commands
  20. 19PXP Demo Guide
    1. 19.1 Demo Overview
    2. 19.2 Demo Application
    3. 19.3 Applications Commands
  21. 20FMP Demo Guide
    1. 20.1 Demo Overview
    2. 20.2 Demo Application
    3. 20.3 Application Commands
  22. 21CSCP Demo Guide
    1. 21.1 Demo Overview
    2. 21.2 Demo Application
    3. 21.3 Application Commands
  23. 22Revision History

Demo Overview

The Hands free profile allows the user to demonstrate the use of Hands-free profile on an embedded device. The hands free profile is used to connect a headset or speakerphone with a mobile device to provide remote control and voice connections. The Hands-free profile supports two roles, Hands free and Audio Gateway. This document demonstrates how to use the hands free role of the profile.

Note: An external codec MUST be connected to the CC256x I2S/PCM interface to play and record audio. The same instructions can be used to run this demo on the MSP430 Platform.
Running the Bluetooth Code

Once the code is flashed, connect the board to a PC using a miniUSB or microUSB cable. Once connected, wait for the driver to install. It will show up as MSP-EXP430F5438 USB - Serial Port(COM x), Tiva Virtual COM Port (COM x) under Ports (COM & LPT) in the Device manager. Attach a Terminal program like PuTTY to the serial port x for the board. The serial parameters to use are 115200 Baud (9600 for MSP430), 8, n, 1. Once connected, reset the device using Reset S3 button (located next to the mini USB connector for the MSP430) and you should see the stack getting initialized on the terminal and the help screen will be displayed, which shows all of the commands.