SPRUIK4A September 2018 – June 2019 TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28076 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S
The SFRA library is distributed through the C2000WARE-DIGITALPOWER-SDK installer, which can be downloaded at http://www.ti.com/tool/C2000WARE-DIGITALPOWER-SDK , alternatively it may be available as part of other SDKs for C2000 MCUs that use SFRA library. By default, the installation places the library components in the following directory structure:
C:\ti\c2000\C2000Ware_DigitalPower_SDK_<version>\libraries\sfra
The following sub-directory structure is shown in Table 1.
| <base>\docs | Documentation |
| <base>\examples | Contains example projects for quickly evaluating SFRA (Software Test Bench). Currently one example inclued is example1_stb which is a software check for the SFRA library. |
| <base>\gui | Host side graphical user interface (SFRA_GUI.exe) that is used for displaying the frequency response and the GUI tool Compensation Designer (ComDesigner.exe) that can be used to design compensator based with the SFRA measured plant information. The SFRAData.csv file is also stored here. |
| <base>\include | Contains the header file that is needed to be included in the system project to use this libarary. |
| <base>\lib | The library file for float32 and float32+TMU processor options. |
| <base>\scripts | Scripts to import SFRA data for compensation design in MATLAB. |
| <base> | Software manifest with version number of the library. |