SPRUIF3B May 2017 – March 2019
For nonvolatile storage expansion, the EVM includes a microSD card cage. The cage is connected to the MMC1 port of the SoC. To support higher-speed cards that operate at lower voltages, the I/O supplies are changed from 3v3 to 1v8 by setting GPIO7_11 to low. The SD card power can be cycled using I/O expander (EXP2 and PP5). See the data manual for the SoC for specific information regarding supported card types, densities, and speeds.
Booting from the microSD card cage is supported on the EVM. No EVM configuration is required as the QSPI flash is enabled by default. Ensure the correct SoC boot mode is set using the SYS_BOOT switches (SW3 and SW4).