SPRUIF3B May 2017 – March 2019
Figure 22 is part of the SoC pinmux table for DCAN2. The SoC device supports additional functions not shown in the table. The functions shown are intended to reflect those supported on the EVM. These functions include:
Figure 22. SoC Pinmux for DCAN2 MUX L: Selects between DCAN2 header and expansion interface. The selection is made using the I/O expander 2, bit P3, defaulting to onboard DCAN header. Figure 23 shows the MUX diagram for DCAN2 and I2C.
Figure 23. MUX Diagram for DCAN2 and I2C