SPRAC21A June 2016 – June 2019 OMAP-L132 , OMAP-L138 , TDA2E , TDA2EG-17 , TDA2HG , TDA2SG , TDA2SX , TDA3LA , TDA3MV
Lower write performance using SATA iSSD is mainly attributed to the slower flash write speed of the iSSD device. There is no restriction from the TDA2xx and TDA2ex SoC to attain full write speed as specified in the SATA specification.
When using HDD and the file system, it is observed that there is marginal lower SATA write performance than read performance. This is as expected as the HDD drive write has higher seek time than reads and other file system write overheads.