SPRAA85E November   2005  – December 2017 F28377D-SEP , SM320F2812 , SM320F2812-EP , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F2801 , TMS320F2801-Q1 , TMS320F2802 , TMS320F2802-Q1 , TMS320F28044 , TMS320F2806 , TMS320F2806-Q1 , TMS320F28062 , TMS320F28062-Q1 , TMS320F28062F , TMS320F28062F-Q1 , TMS320F28063 , TMS320F28064 , TMS320F28065 , TMS320F28066 , TMS320F28066-Q1 , TMS320F28067 , TMS320F28067-Q1 , TMS320F28068F , TMS320F28068M , TMS320F28069 , TMS320F28069-Q1 , TMS320F28069F , TMS320F28069F-Q1 , TMS320F28069M , TMS320F28069M-Q1 , TMS320F28075 , TMS320F28075-Q1 , TMS320F2808 , TMS320F2808-Q1 , TMS320F2809 , TMS320F2810 , TMS320F2810-Q1 , TMS320F2811 , TMS320F2811-Q1 , TMS320F2812 , TMS320F2812-Q1 , TMS320F28232 , TMS320F28232-Q1 , TMS320F28234 , TMS320F28234-Q1 , TMS320F28235 , TMS320F28235-Q1 , TMS320F28332 , TMS320F28333 , TMS320F28334 , TMS320F28335 , TMS320F28335-Q1 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320R2811

 

  1.   Programming TMS320x28xx and TMS320x28xxx Peripherals in C/C++
    1.     Trademarks
    2. Introduction
    3. Traditional #define Approach
      1.      Example 1. Traditional #define Macros
      2.      Example 2. Accessing Registers Using #define Macros
    4. Bit Field and Register-File Structure Approach
      1. 3.1 Defining A Register-File Structure
        1.       Example 3. SCI Register-File Structure Definition
        2.       Example 4. SCI Register-File Structure Variables
      2. 3.2 Using the DATA_SECTION Pragma to Map a Register-File Structure to Memory
        1.       Example 5. Assigning Variables to Data Sections
        2.       Example 6. Mapping Data Sections to Register Memory Locations
        3.       Example 7. Accessing a Member of the SCI Register-File Structure
      3. 3.3 Adding Bit-Field Definitions
        1.       Example 8. SCI Control Registers Defined Using Bit Fields
      4. 3.4 Using Unions
        1.       Example 9. Union Definition to Provide Access to Bit Fields and the Whole Register
        2.       Example 10. SCI Register-File Structure Using Unions
        3.       Example 11. Accessing Bit Fields in C/C++
    5. Bit Field and Register-File Structure Advantages
    6. Code Size and Performance Using Bit Fields
      1.      Example 12. TMS320x280x PCLKCR0 Bit-Field Definition
      2.      Example 13. Assembly Code Generated by Bit Field Accesses
      3.      Example 14. Optimization Using the .all Union Member
      4.      Example 15. Optimization Using a Shadow Register
    7. Read-Modify-Write Considerations When Using Bit Fields
      1.      Example 16. A Few Read-Modify-Write Operations
      2. 6.1 Registers That Hardware Can Modify During Read-Modify-Write Operations
        1. 6.1.1 PIEIFRx Registers
          1.        Example 17. Clearing PIEIFRx (x = 1, 2...12) Registers
        2. 6.1.2 GPxDAT Registers
          1.        Example 18. Read-Modify-Write Effects on GPxDAT Registers
          2.        Example 19. Using GPxSET and GPxCLEAR Registers
      3. 6.2 Registers With Write 1-to-Clear Bits.
        1.       Example 20. Read-Modify-Write Operation Inadvertently Modifies Write 1-to-Clear Bits (TCR[TIF])
        2.       Example 21. Using a Shadow Register to Preserve Write 1-to-Clear Bits
      4. 6.3 Register Bits Requiring a Specific Value
        1.       Example 22. Watchdog Check Bits (WDCR[WDCHK])
      5. 6.4 Read-Modify-Write Sensitive Registers
    8. Special Case Peripherals
      1. 7.1 eCAN Control Registers
        1.       Example 23. Invalid eCAN Control Register 16-Bit Write
        2.       Example 24. Using a Shadow Register to Force a 32-Bit Access
      2. 7.2 Byte Peripheral Registers
        1.       Example 25. Invalid Byte Peripheral Register Access
        2.       Example 26. Byte Peripheral Register Access Using “byte_peripheral” Attribute
    9. C2000 Peripheral Driver Library Approach
      1. 8.1 Using the Peripheral Driver Library
        1.       Example 27. SCI-A Driverlib Function Prototype
          1.        Example 28. SCI-A Configuration Using the Driverlib
      2. 8.2 Construction of a Driver Library Function
        1.       Example 29. SCI Register Description Header File (hw_sci.h)
          1.        Example 30. SCI Function Implementation
      3. 8.3 Peripheral Driver Library Advantages
    10. Code Size and Performance Using Driverlib
      1.      Example 31. Inlined ADC_readResult() Function Calls
      2.      Example 32. ADC Function Implementation to be Optimized
      3.      Example 33. Inlined ADC_setupSOC() Function Call
    11. 10 Comparing and Combining Approaches
      1.      Example 34. CPU Timer Bit-Field (Left) and Driverlib (Right) Disassembly Comparison
      2.      Example 35. ADC Bit-Field (Left) and Driverlib (Right) Disassembly Comparison
    12. 11 References
  2.   Revision History

Example 1. Traditional #define Macros

/******************************************************************** * Traditional header file ********************************************************************/ #define Uint16 unsigned int #define Uint32 unsigned long // Memory Map // Addr Register #define SCICCRA (volatile Uint16 *)0x7050 // 0x7050 SCI-A Communications Control #define SCICTL1A (volatile Uint16 *)0x7051 // 0x7051 SCI-A Control Register 1 #define SCIHBAUDA (volatile Uint16 *)0x7052 // 0x7052 SCI-A Baud Register, High Bits #define SCILBAUDA (volatile Uint16 *)0x7053 // 0x7053 SCI-A Baud Register, Low Bits #define SCICTL2A (volatile Uint16 *)0x7054 // 0x7054 SCI-A Control Register 2 #define SCIRXSTA (volatile Uint16 *)0x7055 // 0x7055 SCI-A Receive Status #define SCIRXEMUA (volatile Uint16 *)0x7056 // 0x7056 SCI-A Receive Emulation Data Buffer #define SCIRXBUFA (volatile Uint16 *)0x7057 // 0x7057 SCI-A Receive Data Buffer #define SCITXBUFA (volatile Uint16 *)0x7059 // 0x7059 SCI-A Transmit Data Buffer #define SCIFFTXA (volatile Uint16 *)0x705A // 0x705A SCI-A FIFO Transmit #define SCIFFRXA (volatile Uint16 *)0x705B // 0x705B SCI-A FIFO Receive #define SCIFFCTA (volatile Uint16 *)0x705C // 0x705C SCI-A FIFO Control #define SCIPRIA (volatile Uint16 *)0x705F // 0x705F SCI-A Priority Control #define SCICCRB (volatile Uint16 *)0x7750 // 0x7750 SCI-B Communications Control #define SCICTL1B (volatile Uint16 *)0x7751 // 0x7751 SCI-B Control Register 1 #define SCIHBAUDB (volatile Uint16 *)0x7752 // 0x7752 SCI-B Baud Register, High Bits #define SCILBAUDB (volatile Uint16 *)0x7753 // 0x7753 SCI-B Baud Register, Low Bits #define SCICTL2B (volatile Uint16 *)0x7754 // 0x7754 SCI-B Control Register 2 #define SCIRXSTB (volatile Uint16 *)0x7755 // 0x7755 SCI-B Receive Status #define SCIRXEMUB (volatile Uint16 *)0x7756 // 0x7756 SCI-B Receive Emulation Data Buffer #define SCIRXBUFB (volatile Uint16 *)0x7757 // 0x7757 SCI-B Receive Data Buffer #define SCITXBUFB (volatile Uint16 *)0x7759 // 0x7759 SCI-B Transmit Data Buffer #define SCIFFTXB (volatile Uint16 *)0x775A // 0x775A SCI-B FIFO Transmit #define SCIFFRXB (volatile Uint16 *)0x775B // 0x775B SCI-B FIFO Receive #define SCIFFCTB (volatile Uint16 *)0x775C // 0x775C SCI-B FIFO Control #define SCIPRIB (volatile Uint16 *)0x775F // 0x775F SCI-B Priority Control

Each macro definition can then be used as a pointer to the register's location as shown in Example 2.