SNLU232A August 2018 – May 2019 DS90UB949A-Q1 , DS90UH949A-Q1
Make sure all the software has been installed and the hardware is powered on and connected to the PC. Execute “Analog LaunchPAD” shortcut from the start menu. The default start menu location is under All Programs → Texas Instruments → Analog LaunchPAD vx.x.x → Analog LaunchPAD to start MainGUI.exe.
The application should come up in the state shown in Figure 1-5. If it does not, see Section 1.12, “Troubleshooting ALP Software”.
NOTE
The ALP window graphics in this document show "DS90UH949", and the document text refers to the DS90Ux949. Replace the "DS90Ux949" text with "DS90UH949" if you have the DS90UH949A-Q1EVM or "DS90UB949" if you have the DS90UB949A-Q1EVM.
Under the Devices tab, select “DS90UH949” for the DS90UB949A-Q1EVM or "DS90UB949" for the DS90UB949A-Q1EVM to open up the device profile with its associated tabs.
After selecting the DS90Ux949, the screen shown in Figure 1-6 should appear.