SNLU232A August   2018  – May 2019

 

  1. 1DS90UH949A-Q1EVM or DS90UB949A-Q1EVM User's Guide
    1. 1.1  General Description
    2. 1.2  Features
    3. 1.3  System Requirements
    4. 1.4  Contents of the Demo Evaluation Kit
    5. 1.5  Applications Diagram
    6. 1.6  Typical Configuration
    7. 1.7  Quick Start Guide
    8. 1.8  Default Jumper Settings
    9. 1.9  Default Switch Settings
    10. 1.10 Demo Board Connections
    11. 1.11 ALP Software Setup
      1. 1.11.1  System Requirements
      2. 1.11.2  Download Contents
      3. 1.11.3  Installation of the ALP Software
      4. 1.11.4  Start-Up - Software Description
      5. 1.11.5  Information Tab
      6. 1.11.6  HDMI Tab
      7. 1.11.7  Pattern Generator Tab
      8. 1.11.8  Registers Tab
      9. 1.11.9  Registers Tab - Address 0x00 Selected
      10. 1.11.10 Registers Tab - Address 0x00 Expanded
      11. 1.11.11 Scripting Tab
    12. 1.12 Troubleshooting ALP Software
      1. 1.12.1 ALP Loads the Incorrect Profile
      2. 1.12.2 ALP Does Not Detect the EVM
    13. 1.13 Typical Connection and Test Equipment
    14. 1.14 Equipment References
    15. 1.15 Cable References
  2. 2Bill of Materials
    1.     A EVM PCB Schematics
      1.      Board Layout
        1.       Board Layers
          1.        Revision History

ALP Does Not Detect the EVM

If the window shown in Figure 1-18 opens after starting the ALP software, double check the hardware setup.

ALP_no_devices_error.gifFigure 1-18 ALP No Devices Error
  1. Check the device manager to make sure that the USB driver is installed. There should be a “HID-compliant device” under the “Human Interface Devices” as shown in Figure 1-19.
  2. windows_7_ALP_USB_driver.gifFigure 1-19 Windows 7, ALP USB Driver
  3. Check to make sure the software starts with only “DS90Ux949” in the “Devices” drop-down menu. If there are more devices then the software is most likely in demo mode. When the ALP is operating in demo mode there is a “(Demo Mode)” indication in the lower left of the application status bar as shown in Figure 1-20.
  4. 949_ALP_demo_mode_snlu169.pngFigure 1-20 ALP in Demo Mode
  5. Select the “Preferences” drop-down menu and un-check the “Enable Demo Mode” check mark to disable the demo mode.
  6. ALP_preferences_menu.gifFigure 1-21 ALP Preferences Menu

After demo mode is disabled, the ALP software will poll the ALP hardware. The ALP software will update and only have “DS90UH949” or "DS90UB949" under the “Devices” drop-down menu.