ZHCSKT9C January 2020 – March 2021 THP210
PRODUCTION DATA
A common application use case for fully-differential amplifiers is to easily convert a single-ended signal into a differential signal to drive a differential input source, such as an ADC or class D amplifier. Figure 9-12 shows an example of the THP210 used to convert a single-ended, low-voltage signal source, such as a small electric microphone, and deliver a low-noise differential signal that is common-mode shifted to the center of the ADC input range. A multiple-feedback (MFB) configuration is used to provide a Butterworth filter response, giving a 40‑dB/decade cutoff with a –3-dB frequency of 30 kHz.
Figure 9-10 Example 30-kHz Butterworth Filter