SPRUIG8I January 2018 – December 2023
To invoke the library information archiver, enter:
libinfo7x [options] --output=libname libname1 [libname2 ... libnamen ] |
libinfo7x |
is the command that invokes the library information archiver. | |
options | changes the default behavior of the library information archiver. These options are: | |
--output libname | specifies the name of the index library to create or update. This option is required. | |
--update | updates any existing information in the index library specified with the --output option instead of creating a new index. | |
libnames | names individual object file libraries to be manipulated. When you enter a libname, you must enter a complete filename including extension, if applicable. |