SPRUIG8I January 2018 – December 2023
In the <stdio.h> header file, the value for the macro FOPEN_MAX has the value of the macro _NFILE, which is set to 10. The impact is that you can only have 10 files simultaneously open at one time (including the pre-defined streams - stdin, stdout, stderr).
The C standard requires that the minimum value for the FOPEN_MAX macro is 8. The macro determines the maximum number of files that can be opened at one time. The macro is defined in the stdio.h header file and can be modified by changing the value of the _NFILE macro and recompiling the library.