SPRUIG8I January 2018 – December 2023
Figure 1-1 illustrates the software development flow. The shaded portion of the figure highlights the most common path of software development for C language programs. The other portions are peripheral functions that enhance the development process.
The following list describes the tools that are shown in Figure 1-1:
The library-build utility automatically builds the run-time-support library if compiler and linker options require a custom version of the library. See Section 7.4. Source code for the standard run-time-support library functions for C and C++ is provided in the lib\src subdirectory of the directory where the compiler is installed.
In addition, the following utilities are provided to help examine or manage the content of a given object file: