SPRUIG8I January 2018 – December 2023
When optimizing with the --opt_level=3 option (aliased as -O3), the compiler automatically inlines small functions. A command-line option, --auto_inline=size, specifies the size threshold for automatic inlining. This option controls only the inlining of functions that are not explicitly declared as inline.
When the --auto_inline option is not used, the compiler sets the size limit based on the optimization level and the optimization goal (performance versus code size). If the -auto_inline size parameter is set to 0, automatic inline expansion is disabled. If the --auto_inline size parameter is set to a non-zero integer, the compiler automatically inlines any function smaller than size. (This is a change from previous releases, which inlined functions for which the product of the function size and the number of calls to it was less than size. The new scheme is simpler, but will usually lead to more inlining for a given value of size.)
The compiler measures the size of a function in arbitrary units; however the optimizer information file (created with the --gen_opt_info=1 or --gen_opt_info=2 option) reports the size of each function in the same units that the --auto_inline option uses. When --auto_inline is used, the compiler does not attempt to prevent inlining that causes excessive growth in compile time or size; use with care.
When --auto_inline option is not used, the decision to inline a function at a particular call-site is based on an algorithm that attempts to optimize benefit and cost. The compiler inlines eligible functions at call-sites until a limit on size or compilation time is reached.
Inlining behavior varies, depending on which compile-time options are specified:
For information about interactions between command-line options, pragmas, and keywords that affect inlining, see Section 3.10.