SPRUIG8I January 2018 – December 2023
Pointer to data member objects are stored in memory like an unsigned int (64-bit) integral type. Its value is the byte offset to the data member in the class, plus 1. The zero value is reserved to represent the NULL pointer.