SPRUIG8I January 2018 – December 2023
The <far_call_trampoline_list> is a list of <far_call_trampoline> elements. The linker supports the generation of far call trampolines to help a call site reach a destination that is out of range. A far call trampoline function is guaranteed to reach the called function (callee) as it may utilize an indirect call to the called function.
The <far_call_trampoline_list> enumerates all of the far call trampolines that are generated by the linker for a particular link. The <far_call_trampoline_list> can contain any number of <far_call_trampoline> elements. Each <far_call_trampoline> is a container enclosing the following elements:
<far_call_trampoline_list>
...
<far_call_trampoline>
<callee_name>_foo</callee_name>
<callee_address>0x08000030</callee_address>
<trampoline_object_component_ref idref="oc-123"/>
<trampoline_address>0x2020</trampoline_address>
<caller_list>
<call_site>
<caller_address>0x1800</caller_address>
<caller_object_component_ref idref="oc-23"/>
</call_site>
<call_site>
<caller_address>0x1810</caller_address>
<caller_object_component_ref idref="oc-23"/>
</call_site>
</caller_list>
</far_call_trampoline>
...
</far_call_trampoline_list>