ZHCSHC3B january 2018 – june 2023 TPS61280D , TPS61280E , TPS61281D
PRODUCTION DATA
PIN | I/O | DESCRIPTION | |
---|---|---|---|
NAME | NO. | ||
VIN | A3, A4 | I | Power supply input. |
VOUT | B3, B4 | O | Boost converter output. |
EN | A1 | I | This is the enable pin of the device. On the rising edge of the enable pin, all the registers are reset with their default values. This input must not be left floating and must be terminated. |
EN = Low: The device is forced into shutdown mode and the I2C control interface is disabled. Depending on the logic level applied to the nBYP input, the converter can either be forced in pass-through mode or it's output can be regulated to a minimum level so as to limit the input-to-output voltage difference to less than 3.6V (typ). The current consumption is reduced to a few µA. For more details, refer to Table 9-2. | |||
EN = High: The device is operating normally featuring automatic dc/dc boost, pass-through mode transition. For more details, refer to Table 9-2. | |||
GPIO | A2 | I/O | This pin can either be configured as a input (mode selection) or as dual role input/open-drain output RST/ FAULT ) pin. For TPS61280D, default configuration is RST/ FAULT input/output. For TPS61280E, default configuration is mode selection input. The input must not be left floating and must be terminated. |
Manual Reset Input: Drive RST/ FAULT low to initiate a reset of the converter's output. nRST/nFAULT controls a falling edge-triggered sequence consisting of a discharge phase of the capacitance located at the converter's output followed by a start-up phase. | |||
Fault Output (open-drain interrupt signal to host): Indicates that a fault has occurred (e.g. thermal shutdown, output voltage out of limits, current limit triggered, and so on). To signal such an event, the device generates a falling edge-triggered interrupt by driving a negative pulse onto the GPIO line and then releases the line to its inactive state. | |||
Mode selection input = Low: The device is operating in regulated frequency pulse width modulation mode (PWM) at high-load currents and in pulse frequency modulation mode (PFM) at light load currents. | |||
Mode selection input = High: Low-noise mode enabled, regulated frequency PWM operation forced. | |||
VSEL | B1 | I | VSEL signal is primarily used to set the output voltage dc/dc boost, pass-through threshold. This pin must not be left floating and must be terminated. |
nBYP | C1 | I | A logic low level on the BYP input forces the device in pass-through mode. This pin must not be left floating and must be terminated. |
SCL | B2 | I | Serial interface clock line. This pin must not be left floating and must be terminated. |
SDA | C2 | I/O | Serial interface address/data line. This pin must not be left floating and must be terminated. |
SW | C3, C4 | I/O | Inductor connection. Drain of the internal power MOSFET. Connect to the switched side of the inductor. |
PGND | D2, D3, D4 | Power ground pin. | |
AGND | D1 | Analog ground pin. This is the signal ground reference for the IC. |
PIN | I/O | DESCRIPTION | |
---|---|---|---|
NAME | NO. | ||
VIN | A3, A4 | I | Power supply input. |
VOUT | B3, B4 | O | Boost converter output. |
EN | A1 | I | This is the enable pin of the device. On the rising edge of the enable pin, all the registers are reset with their default values. This input must not be left floating and must be terminated. |
EN = Low: The device is forced into shutdown mode. Depending on the logic level applied to the nBYP input, the converter can either be forced in pass-through mode or it's output can be regulated to a minimum level so as to limit the input-to-output voltage difference to less than 3.6V (typ). The current consumption is reduced to a few µA. For more details, refer to Table 9-2. | |||
EN = High: The device is operating normally featuring automatic dc/dc boost, pass-through mode transition. For more details, refer to Table 9-2. | |||
PG | A2 | O | Power-Good Output (open-drain output to host): A logic high on the PG output indicates that the converter's output voltage is within its regulation limits. A logic low indicates a fault has occurred (e.g. thermal shutdown, output voltage out of limits, current limit triggered, and so on). The PG signal is de-asserted automatically once the IC resumes proper operation. |
VSEL | B1 | I | VSEL signal is primarily used to set the output voltage dc/dc boost, pass-through threshold. This pin must not be left floating and must be terminated. |
nBYP | C1 | I | A logic low level on the BYP input forces the device in pass-through mode. For more details, refer to Table 9-2. This pin must not be left floating and must be terminated. |
MODE | B2 | I | This is the mode selection pin of the device. This pin must not be left floating, must be terminated and can be connected to AGND. During start-up this pin must be held low. Once the output voltage settled and PG pin indicates that the converter's output voltage is within its regulation limits the device can be forced in PWM mode operation by applying a high level on this pin. |
MODE = Low: The device is operating in regulated frequency pulse width modulation mode (PWM) at high-load currents and in pulse frequency modulation mode (PFM) at light load currents. This pin must be held low during device start-up. | |||
MODE = High: Low-noise mode enabled, regulated frequency PWM operation forced. | |||
SW | C3, C4 | I/O | Inductor connection. Drain of the internal power MOSFET. Connect to the switched side of the inductor. |
PGND | D2, D3, D4 | Power ground pin. | |
AGND | C2, D1 | Analog ground pin. This is the signal ground reference for the IC. |