ZHCSFP7B November 2016 – February 2019 TAS2557
PRODUCTION DATA.
See the General I2C Operation section for more details on addressing. Register settings should be set based on the files generated from the PPC3 GUI. Because the TAS2557 is a complex system including the internal software, changes made in the TAS2557 registers not known in the PPC3 generated configurations can result in the speaker protection not operating correctly. Changes should be made from within PurePath Console 3 Software TAS2557 Application instead of manually changing registers when possible. Configuration files with needed options can be generated from PPC3 to prevent invalid configurations.