ZHCU837 December 2021
The TLV9061 is a single low-voltage op amp with rail-to-rail input- and output-swing capabilities. This device translates the DRV5056 voltage into a voltage that changes the brightness of an LED on the board based on how far the trigger is pressed. The device was selected because of its low cost. Since this device is mainly used for demonstrating the trigger movement with the LED, note that it is not actually needed in a final implementation of a cordless power tool.