SWRA671 June   2020 CC1312R , CC1312R , CC1352P , CC1352P , CC1352R , CC1352R , CC2652P , CC2652P , CC2652R , CC2652R , CC2652R7 , CC2652R7 , CC2652RB , CC2652RB , CC2652RSIP , CC2652RSIP

 

  1.   Cloning Z-Stack Network Properties Using the SimpleLink Wireless MCU Family
    1.     Trademarks
    2. Introduction
    3. Abbreviations and Acronyms
    4. Tool Versions
      1. 3.1 Command Line Interface (CLI)
      2. 3.2 MAC OS Application
      3. 3.3 Windows Executable
    5. Trust Center and Non-Volatile Memory
    6. Multi-Page NVM
    7. MT Interface
    8. Zigbee Coordinator Setup Procedure
    9. Zigbee Coordinator Cloning Procedure
      1. 8.1 Cloning: Method One
      2. 8.2 Cloning: Method Two
    10. Zigbee Coordinator Cloning Procedure Example
    11. 10 Other Application Considerations
    12. 11 Summary
    13. 12 References
  2.   A TI Zigbee Network Properties Cloning Tool Guide
    1.     A.1 Tool Layout
    2.     A.2 Configuration File
    3.     A.3 Content File
    4.     A.4 Application Selection
    5.     A.5 COM Ports
    6.     A.6 Read Settings
    7.     A.7 Write Settings
    8.     A.8 Output Settings
    9.     A.9 Save/Load Settings
    10.     A.10 Help
  3.   B Establishing a Serial Connection
    1.     B.1 Serial Connections
    2.     B.2 Detecting COM Ports

Zigbee Coordinator Cloning Procedure

The TI Zigbee Network Properties Cloning Tool is an executable that allows the user to clone the existing network properties of a ZC to another ZC. The tool also has the capability to read and write to a ZC device. For details on how to operate the GUI and its functionality, see Section A.

There are two methods that can be used to clone the network properties of a ZC. Method one, described in Section 8.1, requires that both devices be available while the procedure will take place. Method two, described in Section 8.2, should be used when both devices are not available simultaneously.