SWRA671 June 2020 CC1312R , CC1312R , CC1352P , CC1352P , CC1352R , CC1352R , CC2652P , CC2652P , CC2652R , CC2652R , CC2652R7 , CC2652R7 , CC2652RB , CC2652RB , CC2652RSIP , CC2652RSIP
The ‘Read’ option in the application section enables the user to select which items to read from. All NV Regions specified within the configuration file will be visible using the ‘NV Region’ name. If ‘All Regions’ is selected as the option to read then all NV Regions that appear will be read from, else only the selected items will be read from. If there is an error reading a region or there is no content for the region then the tool will not read from the device; if this happens an error message will be displayed in the output display. To view the data that is read from a device go to View -> Read File. Within this file is the NV Region, Item ID, System ID (if any), Sub ID (if any), length of the data read, and the data itself.