SWRA671 June   2020 CC1312R , CC1312R , CC1352P , CC1352P , CC1352R , CC1352R , CC2652P , CC2652P , CC2652R , CC2652R , CC2652R7 , CC2652R7 , CC2652RB , CC2652RB , CC2652RSIP , CC2652RSIP

 

  1.   Cloning Z-Stack Network Properties Using the SimpleLink Wireless MCU Family
    1.     Trademarks
    2. Introduction
    3. Abbreviations and Acronyms
    4. Tool Versions
      1. 3.1 Command Line Interface (CLI)
      2. 3.2 MAC OS Application
      3. 3.3 Windows Executable
    5. Trust Center and Non-Volatile Memory
    6. Multi-Page NVM
    7. MT Interface
    8. Zigbee Coordinator Setup Procedure
    9. Zigbee Coordinator Cloning Procedure
      1. 8.1 Cloning: Method One
      2. 8.2 Cloning: Method Two
    10. Zigbee Coordinator Cloning Procedure Example
    11. 10 Other Application Considerations
    12. 11 Summary
    13. 12 References
  2.   A TI Zigbee Network Properties Cloning Tool Guide
    1.     A.1 Tool Layout
    2.     A.2 Configuration File
    3.     A.3 Content File
    4.     A.4 Application Selection
    5.     A.5 COM Ports
    6.     A.6 Read Settings
    7.     A.7 Write Settings
    8.     A.8 Output Settings
    9.     A.9 Save/Load Settings
    10.     A.10 Help
  3.   B Establishing a Serial Connection
    1.     B.1 Serial Connections
    2.     B.2 Detecting COM Ports

Detecting COM Ports

In order to know which port to use for a machine running on a Windows operating system, connect the device in question to the host computer, and use the ‘Ports (COM & LPT)’ drop down in Device Manager to identify the port number of the device, refer to Figure 5 for an example.

Figure 5. COM Port in Device Managercom-ports-swra671.png