SWRA671 June   2020 CC1312R , CC1312R , CC1314R10 , CC1314R10 , CC1352P , CC1352P , CC1352R , CC1352R , CC1354P10 , CC1354P10 , CC1354R10 , CC1354R10 , CC2652P , CC2652P , CC2652R , CC2652R , CC2652R7 , CC2652R7 , CC2652RB , CC2652RB , CC2652RSIP , CC2652RSIP

 

  1.   Cloning Z-Stack Network Properties Using the SimpleLink Wireless MCU Family
    1.     Trademarks
    2. 1  Introduction
    3. 2  Abbreviations and Acronyms
    4. 3  Tool Versions
      1. 3.1 Command Line Interface (CLI)
      2. 3.2 MAC OS Application
      3. 3.3 Windows Executable
    5. 4  Trust Center and Non-Volatile Memory
    6. 5  Multi-Page NVM
    7. 6  MT Interface
    8. 7  Zigbee Coordinator Setup Procedure
    9. 8  Zigbee Coordinator Cloning Procedure
      1. 8.1 Cloning: Method One
      2. 8.2 Cloning: Method Two
    10. 9  Zigbee Coordinator Cloning Procedure Example
    11. 10 Other Application Considerations
    12. 11 Summary
    13. 12 References
  2.   A TI Zigbee Network Properties Cloning Tool Guide
    1.     A.1 Tool Layout
    2.     A.2 Configuration File
    3.     A.3 Content File
    4.     A.4 Application Selection
    5.     A.5 COM Ports
    6.     A.6 Read Settings
    7.     A.7 Write Settings
    8.     A.8 Output Settings
    9.     A.9 Save/Load Settings
    10.     A.10 Help
  3.   B Establishing a Serial Connection
    1.     B.1 Serial Connections
    2.     B.2 Detecting COM Ports

Write Settings

The ‘Write’ option in the application section enables the user to select which NV items to write. There are two types of writing: from a file or use the tool to manually enter data. To write from a file simply check the 'Write from File' option and upload the desired file. If there was a successful upload then the 'Uploaded' status will appear to the right of the 'Write from File' checkbox. For manual entries, only the NV regions configured without a System ID, Sub ID, and entries field will appear as options for the NV Regions. To write to an NV region simply enter the desired value into the text box for the corresponding region. Data can be entered with a prefix of '0x' or just the data itself in hex representation. If the value written to an NV Region is not of correct length or type then the value will not be written to the NV Region and the user will be prompted of this through the output display.