SWRA671 June   2020 CC1312R , CC1312R , CC1314R10 , CC1314R10 , CC1352P , CC1352P , CC1352R , CC1352R , CC1354P10 , CC1354P10 , CC1354R10 , CC1354R10 , CC2652P , CC2652P , CC2652R , CC2652R , CC2652R7 , CC2652R7 , CC2652RB , CC2652RB , CC2652RSIP , CC2652RSIP

 

  1.   Cloning Z-Stack Network Properties Using the SimpleLink Wireless MCU Family
    1.     Trademarks
    2. 1  Introduction
    3. 2  Abbreviations and Acronyms
    4. 3  Tool Versions
      1. 3.1 Command Line Interface (CLI)
      2. 3.2 MAC OS Application
      3. 3.3 Windows Executable
    5. 4  Trust Center and Non-Volatile Memory
    6. 5  Multi-Page NVM
    7. 6  MT Interface
    8. 7  Zigbee Coordinator Setup Procedure
    9. 8  Zigbee Coordinator Cloning Procedure
      1. 8.1 Cloning: Method One
      2. 8.2 Cloning: Method Two
    10. 9  Zigbee Coordinator Cloning Procedure Example
    11. 10 Other Application Considerations
    12. 11 Summary
    13. 12 References
  2.   A TI Zigbee Network Properties Cloning Tool Guide
    1.     A.1 Tool Layout
    2.     A.2 Configuration File
    3.     A.3 Content File
    4.     A.4 Application Selection
    5.     A.5 COM Ports
    6.     A.6 Read Settings
    7.     A.7 Write Settings
    8.     A.8 Output Settings
    9.     A.9 Save/Load Settings
    10.     A.10 Help
  3.   B Establishing a Serial Connection
    1.     B.1 Serial Connections
    2.     B.2 Detecting COM Ports

Output Settings

The output display contains the ‘Start’ button used to run the program; alternatively, pressing the File -> Start option will also complete the same task. The progress bar to the right of the ‘Start’ button indicates how far a task is from completion. The output display box will deliver status updates for the user as an indication of what is being done or if there are any warnings and or errors. To store the content of this “log” after an operation is complete go to View -> Export Log File.