SWRA671 June   2020 CC1312R , CC1312R , CC1314R10 , CC1314R10 , CC1352P , CC1352P , CC1352R , CC1352R , CC1354P10 , CC1354P10 , CC1354R10 , CC1354R10 , CC2652P , CC2652P , CC2652R , CC2652R , CC2652R7 , CC2652R7 , CC2652RB , CC2652RB , CC2652RSIP , CC2652RSIP

 

  1.   Cloning Z-Stack Network Properties Using the SimpleLink Wireless MCU Family
    1.     Trademarks
    2. 1  Introduction
    3. 2  Abbreviations and Acronyms
    4. 3  Tool Versions
      1. 3.1 Command Line Interface (CLI)
      2. 3.2 MAC OS Application
      3. 3.3 Windows Executable
    5. 4  Trust Center and Non-Volatile Memory
    6. 5  Multi-Page NVM
    7. 6  MT Interface
    8. 7  Zigbee Coordinator Setup Procedure
    9. 8  Zigbee Coordinator Cloning Procedure
      1. 8.1 Cloning: Method One
      2. 8.2 Cloning: Method Two
    10. 9  Zigbee Coordinator Cloning Procedure Example
    11. 10 Other Application Considerations
    12. 11 Summary
    13. 12 References
  2.   A TI Zigbee Network Properties Cloning Tool Guide
    1.     A.1 Tool Layout
    2.     A.2 Configuration File
    3.     A.3 Content File
    4.     A.4 Application Selection
    5.     A.5 COM Ports
    6.     A.6 Read Settings
    7.     A.7 Write Settings
    8.     A.8 Output Settings
    9.     A.9 Save/Load Settings
    10.     A.10 Help
  3.   B Establishing a Serial Connection
    1.     B.1 Serial Connections
    2.     B.2 Detecting COM Ports

Tool Versions

The TI Zigbee Network Properties Cloning Tool along with any required files can be found here. There are three separate versions of the tool {CLI, MAC OS, Windows}. This application report focuses on the Windows version of the tool. For more detailed instructions that deal with the operation of the tool, see the device-specific READ ME files under the tool version folder of interest.