SWRA671 June   2020 CC1312R , CC1312R , CC1314R10 , CC1314R10 , CC1352P , CC1352P , CC1352R , CC1352R , CC1354P10 , CC1354P10 , CC1354R10 , CC1354R10 , CC2652P , CC2652P , CC2652R , CC2652R , CC2652R7 , CC2652R7 , CC2652RB , CC2652RB , CC2652RSIP , CC2652RSIP

 

  1.   Cloning Z-Stack Network Properties Using the SimpleLink Wireless MCU Family
    1.     Trademarks
    2. 1  Introduction
    3. 2  Abbreviations and Acronyms
    4. 3  Tool Versions
      1. 3.1 Command Line Interface (CLI)
      2. 3.2 MAC OS Application
      3. 3.3 Windows Executable
    5. 4  Trust Center and Non-Volatile Memory
    6. 5  Multi-Page NVM
    7. 6  MT Interface
    8. 7  Zigbee Coordinator Setup Procedure
    9. 8  Zigbee Coordinator Cloning Procedure
      1. 8.1 Cloning: Method One
      2. 8.2 Cloning: Method Two
    10. 9  Zigbee Coordinator Cloning Procedure Example
    11. 10 Other Application Considerations
    12. 11 Summary
    13. 12 References
  2.   A TI Zigbee Network Properties Cloning Tool Guide
    1.     A.1 Tool Layout
    2.     A.2 Configuration File
    3.     A.3 Content File
    4.     A.4 Application Selection
    5.     A.5 COM Ports
    6.     A.6 Read Settings
    7.     A.7 Write Settings
    8.     A.8 Output Settings
    9.     A.9 Save/Load Settings
    10.     A.10 Help
  3.   B Establishing a Serial Connection
    1.     B.1 Serial Connections
    2.     B.2 Detecting COM Ports

Save/Load Settings

Within the Tools menu tab is the option to save and load settings. Saving the settings enables the user to store all of the selections and entries made so that they may be pre-loaded at a different point in time. When loading the settings choose the file which was created from saving the settings. If there is an error with this process then the error message will be shown in the output display.