SWRA478D February 2015 – January 2019 CC1310 , CC1312PSIP , CC1312R , CC1314R10 , CC1352P , CC1352P7 , CC1352R , CC2640 , CC2640R2F , CC2640R2F-Q1 , CC2642R , CC2642R-Q1 , CC2650 , CC2650MODA , CC2652P , CC2652R , CC2652R7 , CC2652RB , CC2652RSIP
To get a clean current measurement, the jumpers on the LaunchPad should be removed. The CC2652R Launchpad with all jumpers removed is shown in Figure 5-2. Note that when the JTAG jumpers are removed, the programming and debug capabilities of the chip become unavailable. This is also applicable for the other CC26xx and CC13xx LaunchPads ([17] - [21]).
Figure 5-2 CC2652R LaunchPad Jumper Removal